• AVR Freaks

How can create timer in uart/usart interrupt

Author
kishanpatel
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2019/01/08 05:47:17
  • Location: 0
  • Status: offline
2019/09/14 00:02:05 (permalink)
0

How can create timer in uart/usart interrupt

Hello,
        I have using ATSAM4S16C module. Actually, i have to call some function when receive any particular data in uart/usart interrupt. I can see that particular data has been received in uart/usart interrupt, but i cant create timer at there. So, how can i call any function/create timer in uart interrupt?
 
Regards,
Kishan Patel.
#1
Jump to:
© 2020 APG vNext Commercial Version 4.5