• AVR Freaks

Interrupt with Change Notification pins[solved]

Author
PS225
New Member
  • Total Posts : 23
  • Reward points : 0
  • Joined: 2018/08/26 22:39:53
  • Location: 0
  • Status: offline
2019/09/10 23:39:53 (permalink)
0

Interrupt with Change Notification pins[solved]

Hello
I am using PIC32MX795F512L(with harmony), and i wanted to use two GPIO pins as an interrupt . I have designed my own board. I dont have any INTx pins available(or free to use). I need to check two pins for their rising edge and accordingly perform some operation. Can i use the change notification feature here?? If so, can anyone please help me with the concept and code??
 
Thanks 
post edited by PS225 - 2019/09/11 00:30:22
#1

1 Reply Related Threads

    ric
    Super Member
    • Total Posts : 23535
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: Interrupt with Change Notification pins[solved] 2019/09/11 19:21:30 (permalink)
    4 (1)
    So is the problem now solved, as your edited subject line seems to indicate?
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    Jump to:
    © 2019 APG vNext Commercial Version 4.5