• AVR Freaks

Hot!Multiple ICD3s using Command Line

Author
Erik_S
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2019/09/09 07:44:57
  • Location: 0
  • Status: offline
2019/09/10 09:47:40 (permalink)
0

Multiple ICD3s using Command Line

Hello
For the last 3 years we used Labview and Command script to program the switches using ICD3. Unfortunately it takes 23 sec each program. Just recently we changed a chip to use a Microchip PIC18LF26K40 chip for one of our new joysticks. This takes program time to sometimes 1 min each. To counter this program time problem we wanted to run 2 ICD3s at the same time. The GUI has the option to select the device.  Is there a way to select the ICD3 using command line. 
#1

6 Replies Related Threads

    Sudheer Herle
    Super Member
    • Total Posts : 425
    • Reward points : 0
    • Joined: 2012/03/30 05:41:29
    • Location: Bangalore ,India
    • Status: offline
    Re: Multiple ICD3s using Command Line 2019/09/11 08:19:33 (permalink)
    0
    You should be able to specify icd3 using serial number too. Check the documentation.
    #2
    Erik_S
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2019/09/09 07:44:57
    • Location: 0
    • Status: offline
    Re: Multiple ICD3s using Command Line 2019/09/11 09:28:04 (permalink)
    0
    I read the documents found in v3.15 v4.20 and v5.05.
    There is no mention of ICD3 tool selection
    #3
    ric
    Super Member
    • Total Posts : 27716
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: Multiple ICD3s using Command Line 2019/09/11 18:18:54 (permalink)
    0
    I think NorthGuy's programmers could do it in about 5 seconds.
    https://www.northernsoftware.com/nsdsp/
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #4
    NorthGuy
    Super Member
    • Total Posts : 6185
    • Reward points : 0
    • Joined: 2014/02/23 14:23:23
    • Location: Northern Canada
    • Status: offline
    Re: Multiple ICD3s using Command Line 2019/09/15 08:33:05 (permalink)
    0
    ric
    I think NorthGuy's programmers could do it in about 5 seconds.



    5 sec is very close. It is 3.8 sec:
     
    https://www.northernsoftware.com/dev/pic18f/pic18f26k40.htm
     
    However. It'll be faster if you do not program EEPROM, which is very slow to program compared to program flash.
     
     
    #5
    aschen0866
    Super Member
    • Total Posts : 4567
    • Reward points : 0
    • Joined: 2006/01/08 22:18:32
    • Location: San Diego
    • Status: offline
    Re: Multiple ICD3s using Command Line 2019/09/15 09:33:51 (permalink)
    5 (1)
    Erik_S
    I read the documents found in v3.15 v4.20 and v5.05.
    There is no mention of ICD3 tool selection


    From Readme for IPECMD.htm, 

    T
    P = Tool Selection E.g. –TPRICE for MPLAB REAL ICE –TPPK3 for PICKIT 3
    S = Specific Tool Selection using Serial No, E.g. TSBUR1234566
    Short Name for Tools:
    MPLAB REAL ICE   –  RICE
    MPLAB ICD 4    -  ICD4
    MPLAB ICD 3        –  ICD3
    MPLAB PICkit 4   –  PK4
    PICKIT 3   –  PK3
    MPLAB PM3         –  PM3
    PKOB    -  PKOB

    #6
    tech24x7
    Junior Member
    • Total Posts : 97
    • Reward points : 0
    • Joined: 2013/10/14 21:38:52
    • Location: 0
    • Status: offline
    Re: Multiple ICD3s using Command Line 2019/10/29 02:16:06 (permalink)
    0
    You can move to Gen4 Tools that much much faster than Gen3.  Please try PK4.
    #7
    Jump to:
    © 2020 APG vNext Commercial Version 4.5