• AVR Freaks

PIC32MZ EF Harmony3 SQICS1 used by default

Author
Luca Pascarella
Starting Member
  • Total Posts : 69
  • Reward points : 0
  • Joined: 2007/05/28 00:53:17
  • Location: The Netherlands
  • Status: offline
2019/09/09 10:57:48 (permalink)
5 (1)

PIC32MZ EF Harmony3 SQICS1 used by default

I found an issue in the drv_sst26.c Harmony 3 when used with a PIC32MZ. The line SQI_BDCTRL_SQICS_CS1 is used by default and it seems there are no options in Harmony 3 Configurator to use SQICS0 instead of SQICS1.
When every occurrence of SQI_BDCTRL_SQICS_CS1 is substitute with SQI_BDCTRL_SQICS_CS0 the CS0 line work properly.
 
BTW. How to do bugs reports for Harmony 3? Are issues in GitHub monitored by developers?
 
Luca
 
 
#1

1 Reply Related Threads

    optimus_jack
    Starting Member
    • Total Posts : 54
    • Reward points : 0
    • Joined: 2017/02/16 03:02:47
    • Location: 0
    • Status: offline
    Re: PIC32MZ EF Harmony3 SQICS1 used by default 2019/09/09 20:20:03 (permalink)
    0
    Hi,
    That's a Good catch. You can post the issue on github for that repository
    #2
    Jump to:
    © 2019 APG vNext Commercial Version 4.5