• AVR Freaks

Helpful ReplyHot!Confusing language in documentation re "CPU Priority Level" & "interrupt priority level"

Author
ReverseEMF
Starting Member
  • Total Posts : 35
  • Reward points : 0
  • Joined: 2012/03/14 17:30:40
  • Location: 0
  • Status: offline
2019/09/07 22:24:32 (permalink)
0

Confusing language in documentation re "CPU Priority Level" & "interrupt priority level"

The "Sec10. Power-Saving Features" document for PIC24F, in subsection 3 "Instruction-Based Power-Saving Modes", the language is confusing, to me.   In section 10.3.1.6 "WAKE-UP FROM SLEEP ON INTERRUPT", talks about interrupts as assigned to a "CPU priority level".  But, there is also a CPU priority level, set by the IPL bits [4 in all], which, certainly, is a different thing, than an interrupt priority level, like the Change Notification [CNIP], or the Timer2 Interrupt Priority [T2IP].
 
So...why does this document use the term "CPU priority", when it seems to be referring to an IPC style interrupt priority?!?

For instance: "User interrupt sources that are assigned to CPU priority level 0 cannot wake the CPU from Sleep
mode"
OR
"To use an interrupt as a wake-up source, the CPU priority level for the interrupt must be assigned to CPU priority level 1 or greater."
 
How can a regular interrupt have a CPU priority level?!?  Isn't it just a priority level, and isn't CPU priority a different thing?
 
post edited by ReverseEMF - 2019/09/08 07:04:00

The Electrons Flow Round and Round...
#1
NKurzman
A Guy on the Net
  • Total Posts : 18672
  • Reward points : 0
  • Joined: 2008/01/16 19:33:48
  • Location: 0
  • Status: offline
Re: Confusing language in documentation re "CPU Priority Level" & "interrupt priority leve 2019/09/08 00:23:09 (permalink)
5 (1)
The interrupts must have a higher level then the cpu priority level or they will not fire.
Setting the CPU to the highest level effectively disables all interrupts.
#2
NorthGuy
Super Member
  • Total Posts : 6097
  • Reward points : 0
  • Joined: 2014/02/23 14:23:23
  • Location: Northern Canada
  • Status: online
Re: Confusing language in documentation re "CPU Priority Level" & "interrupt priority leve 2019/09/08 05:48:26 (permalink) ☄ Helpfulby ReverseEMF 2019/09/08 11:25:53
5 (1)
BlindedByDaLight
How can a regular interrupt have a CPU priority level?!?



When an ISR is invoked, the CPU priority level becomes equal to the interrupt priority level. It then reverts back when ISR returns. This way lower-priority interrupts are automatically blocked while ISR executes.
#3
ReverseEMF
Starting Member
  • Total Posts : 35
  • Reward points : 0
  • Joined: 2012/03/14 17:30:40
  • Location: 0
  • Status: offline
Re: Confusing language in documentation re "CPU Priority Level" & "interrupt priority leve 2019/09/08 11:24:51 (permalink)
0
Thank you for the replies.
 
I also found the following [suggested in the "Related Threads"], which went a long way towards answering my questions regarding interrupt priority: https://www.microchip.com/forums/m328564.aspx?tree=true
 
 

The Electrons Flow Round and Round...
#4
aschen0866
Super Member
  • Total Posts : 4554
  • Reward points : 0
  • Joined: 2006/01/08 22:18:32
  • Location: San Diego
  • Status: offline
Re: Confusing language in documentation re "CPU Priority Level" & "interrupt priority leve 2019/09/08 11:45:19 (permalink)
0
BlindedByDaLight
How can a regular interrupt have a CPU priority level?!? Isn't it just a priority level, and isn't CPU priority a different thing?


This picture is for a PIC32 but the idea is the same. The CPU's priority level (IPLx) is part of the CPU core design. Then you have an interrupt controller that is outside of the core, which controls interrupt vectors' priority via those IPCx settings. An ISR can only be fired up if the interrupt vector's priority is higher than the current CPU's IPL. In a PIC24, the only way to disable global interrupt including the priority 7 interrupt is to raise the CPU's IPL to 7.
 
In the Single-Vector mode, a CPU always jumps to the same address, whereas in the Multi-Vector mode, the CPU jumps to a specific address based up the vector number.
 
#5
Nikolay_Po
Super Member
  • Total Posts : 1939
  • Reward points : 0
  • Joined: 2012/04/01 13:49:27
  • Location: Russia, Novorossiysk
  • Status: offline
Re: Confusing language in documentation re "CPU Priority Level" & "interrupt priority leve 2019/09/08 14:40:51 (permalink)
0
"User interrupt sources that are assigned to CPU priority level 0 cannot wake the CPU from Sleep
mode"
"To use an interrupt as a wake-up source, the CPU priority level for the interrupt must be assigned to CPU priority level 1 or greater."
I believe the CPU word may be completely omitted from these sentences.
#6
ReverseEMF
Starting Member
  • Total Posts : 35
  • Reward points : 0
  • Joined: 2012/03/14 17:30:40
  • Location: 0
  • Status: offline
Re: Confusing language in documentation re "CPU Priority Level" & "interrupt priority leve 2019/09/17 12:01:52 (permalink)
0
aschen0866
In the Single-Vector mode, a CPU always jumps to the same address, whereas in the Multi-Vector mode, the CPU jumps to a specific address based up the vector number.



If so, then in the Single-Vector mode, how does that "same address" lead to connection to the correct handler?  it seems to me, in both modes, the CPU will jump to the address based on the vector number.  I think "Single-Vector" means one vector at a time, not a single vector destination.

The Electrons Flow Round and Round...
#7
ReverseEMF
Starting Member
  • Total Posts : 35
  • Reward points : 0
  • Joined: 2012/03/14 17:30:40
  • Location: 0
  • Status: offline
Re: Confusing language in documentation re "CPU Priority Level" & "interrupt priority leve 2019/09/17 12:11:30 (permalink)
0
Nikolay_Po
"User interrupt sources that are assigned to CPU priority level 0 cannot wake the CPU from Sleep
mode"
"To use an interrupt as a wake-up source, the CPU priority level for the interrupt must be assigned to CPU priority level 1 or greater."
I believe the CPU word may be completely omitted from these sentences.


That's what I thought, at first, too.  But, now I'm not so sure, since it's the CPU Priority Level that drives Interrupt inclusion or exclusion.  And, because, when an ISR is being executed, the CPU Priority Level actually changes to the Priority of the Interrupt being serviced.  So, if another interrupt occurs, during the ISR [when Nesting is enabled], it's the CPU priority level that is being used to determine whether a concurrent interrupt will be serviced, or ignored.

The Electrons Flow Round and Round...
#8
Nikolay_Po
Super Member
  • Total Posts : 1939
  • Reward points : 0
  • Joined: 2012/04/01 13:49:27
  • Location: Russia, Novorossiysk
  • Status: offline
Re: Confusing language in documentation re "CPU Priority Level" & "interrupt priority leve 2019/09/17 12:36:50 (permalink)
0
BlindedByDaLight
aschen0866
In the Single-Vector mode, a CPU always jumps to the same address, whereas in the Multi-Vector mode, the CPU jumps to a specific address based up the vector number.



If so, then in the Single-Vector mode, how does that "same address" lead to connection to the correct handler?  it seems to me, in both modes, the CPU will jump to the address based on the vector number.  I think "Single-Vector" means one vector at a time, not a single vector destination.


I have not heard about single-vector interrupt controller mode for PIC24-th. May be the quote above is a comparison of mid-range 8-bit PICs with 16-bit PIC24-ths? Using single interrupt vector the programmer must to implement required tests inside of ISR, for example, check interrupt flags. So the difference of code behavior for different interrupt sources may be implemented in software, even at single interrupt vector. It is OK but not so fast and without interrupt nesting which are available starting from PIC24-th.
 
P.S. Hmm... The quote "In the Single-Vector mode, a CPU always jumps to the same address, whereas in the Multi-Vector mode, the CPU jumps to a specific address based up the vector number." is from PIC32 documents. This thread may be inappropriate for certain question.
post edited by Nikolay_Po - 2019/09/17 12:40:22
#9
jtemples
عُضْوٌ جَدِيد
  • Total Posts : 11823
  • Reward points : 0
  • Joined: 2004/02/13 12:31:19
  • Location: Southern California
  • Status: offline
Re: Confusing language in documentation re "CPU Priority Level" & "interrupt priority leve 2019/09/17 12:54:30 (permalink)
0
I think aschen0866  was referring to the PIC32 there, but some PIC24E parts do have a single-vector mode for code running in the auxiliary flash segment.
#10
Jump to:
© 2020 APG vNext Commercial Version 4.5