• AVR Freaks

Hot!VGDD problem

Author
ezedhill
Junior Member
  • Total Posts : 93
  • Reward points : 0
  • Joined: 2019/02/07 06:43:05
  • Location: 0
  • Status: offline
2019/09/07 07:53:37 (permalink)
0

VGDD problem

I installed the legacy libraries. Ran the MPLAB X wizard. Tried to compile the MPLAB X project and this is the error I am seeing. 
 
 
 
post edited by ezedhill - 2019/09/07 07:56:29

Attached Image(s)

#1

7 Replies Related Threads

    Antipodean
    Super Member
    • Total Posts : 1802
    • Reward points : 0
    • Joined: 2008/12/09 10:19:08
    • Location: Didcot, United Kingdom
    • Status: offline
    Re: VGDD problem 2019/09/07 08:03:47 (permalink)
    0
    Why don't you continue your old thread over here 
    https://www.microchip.com/forums/m1110616.aspx
    instead of starting a new one about the same thing?
     

    Do not use my alias in your message body when replying, your message will disappear ...

    Alan
    #2
    ezedhill
    Junior Member
    • Total Posts : 93
    • Reward points : 0
    • Joined: 2019/02/07 06:43:05
    • Location: 0
    • Status: offline
    Re: VGDD problem 2019/09/07 19:38:26 (permalink)
    0
    Because I was trying to post a screenshot of the compile error in MPLAB X. I thought starting a new thread might alleviate the problem. But same thing happens in the post. The strange thing about it, if I remove the screenshot, I can post. 
     
    The following is what I see when I try to post with the screenshot.
     

    Access Denied

    You don't have permission to access "http://www.microchip.com/forums/post.aspx?" on this server.
    Reference #18.5494dc17.1567910253.7db1495
    #3
    ezedhill
    Junior Member
    • Total Posts : 93
    • Reward points : 0
    • Joined: 2019/02/07 06:43:05
    • Location: 0
    • Status: offline
    Re: VGDD problem 2019/09/07 20:41:43 (permalink)
    0
    The error I am getting, GFX_DISPLAY_BUFFER_START_ADDRESS is not declared. This is an address for a buffer. Do I have to initialize this with some address?
     
     
    // initialize the work areas and display buffer base addresses global variables
    _workArea1BaseAddr = GFX_DISPLAY_BUFFER_START_ADDRESS;
    _workArea2BaseAddr = GFX_DISPLAY_BUFFER_START_ADDRESS;
    #4
    Wieschebrock
    Super Member
    • Total Posts : 213
    • Reward points : 0
    • Joined: 2005/01/22 07:57:44
    • Location: Germany
    • Status: offline
    Re: VGDD problem 2019/09/19 06:44:47 (permalink)
    +1 (1)
    There should be a VGDD system_config.h in the project with hardware specific definitions:
     
    (...)
    // GFX_DISPLAY_BUFFER_START_ADDRESS - This defines the constant used to set the location of the display buffer location.
    // for the PIC24FJ256DA210 the address used must be consistent with the "DATA SPACE MEMORY MAP FOR PIC24FJ256DA210 FAMILY DEVICES

    #define GFX_DISPLAY_BUFFER_START_ADDRESS 0x00020000ul
    #define GFX_DISPLAY_BUFFER_LENGTH BUF_SIZE // 0x0004B000ul // This defines the size of the display buffer in bytes.
    #define GFX_EPMP_CS1_BASE_ADDRESS 0x00020000ul
    #define GFX_EPMP_CS1_MEMORY_SIZE 0x00040000ul // G
    (..)

     
     
    #5
    ezedhill
    Junior Member
    • Total Posts : 93
    • Reward points : 0
    • Joined: 2019/02/07 06:43:05
    • Location: 0
    • Status: offline
    Re: VGDD problem 2019/09/19 07:55:40 (permalink)
    0
    Interesting, I see the file, but the lines are not in it! So can I just insert these lines?
    #6
    Wieschebrock
    Super Member
    • Total Posts : 213
    • Reward points : 0
    • Joined: 2005/01/22 07:57:44
    • Location: Germany
    • Status: offline
    Re: VGDD problem 2019/09/20 05:35:37 (permalink)
    0
    What hardware do you have?
    You might run the MPLABX wizard in VGDD (under: "Tools") that creates the system_config. If you have a MC development board or display the generated config should fit perfect. If not, it might be a good starting point to choose a display with similar technical properties.
     
    Btw: VGDD ist open source now. 
    #7
    ezedhill
    Junior Member
    • Total Posts : 93
    • Reward points : 0
    • Joined: 2019/02/07 06:43:05
    • Location: 0
    • Status: offline
    Re: VGDD problem 2019/09/20 06:07:22 (permalink)
    0
    The hardware is the PIC24FJ256DA210 development board and the 3.5" Hewhaven 320x240 that plugs into the development board. I select these two in the VGDD MPLAB wizard. I love the VGDD designer. If it only worked for me. Have you had success with it? When you say open source, do they no longer charge for it. I am using the demo version. Maybe this is the problem. 
    #8
    Jump to:
    © 2020 APG vNext Commercial Version 4.5