• AVR Freaks

Hot!RN4678 SPP COnnection from Raspbian or Ubuntu

Author
tuzumkuru
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2019/09/05 04:57:19
  • Location: 0
  • Status: offline
2019/09/06 02:13:34 (permalink)
0

RN4678 SPP COnnection from Raspbian or Ubuntu

Hello everyone,
 
While designing a new Bluetooth communication board, I've used RN4678 instead of RN42 since it is said that "Not Recommended for new designs".
 
I have my board now and it is working as expected when I connect it from a Serial Port Software through Windows 10. I can send and receive data as expected. 
 
The problem starts when I want to use Raspberry Pi or Ubuntu. When I try to connect to the module by first creating an spp using rfcomm and then connecting to serial port with minicom I can not achieve succesfull connection. I was successfully using this method using RN42.
 
When I create a connection using "sudo rfcomm connect hci0 *MACIDofRN4678*" command, rfcomm connects succesfully but, my module messages these immediately: %CONNECT,*MACIDofUSBBT*%%RFCOMM_OPEN%%RFCOMM_CLOSE%%DISCONN%
 
When I connect to rfcomm0 with minicom using "sudo minicom -D /dev/rfcomm0" command it says it is connected but my RN4678 sends messages as: 
%CONNECT,*MACIDofUSBBT*%%RFCOMM_OPEN%%RFCOMM_CLOSE%%DISCONN%%CONNECT,*MACIDofUSBBT*%%RFCOMM_OPEN%%RFCOMM_CLOSE%%
RFCOMM_OPEN%%RFCOMM_CLOSE%%RFCOMM_OPEN%%RFCOMM_CLOSE%%DISCONN%%CONNECT,*MACIDofUSBBT*%%RFCOMM_OPEN%%RFCOMM_CLO
SE%%RFCOMM_OPEN%%RFCOMM_CLOSE%%RFCOMM_OPEN%%RFCOMM_CLOSE%%DISCONN%%CONNECT,*MACIDofUSBBT*%%RFCOMM_OPEN%%RFCOMM
_CLOSE%%RFCOMM_OPEN%%RFCOMM_CLOSE%%DISCONN%%CONNECT,*MACIDofUSBBT*%%RFCOMM_OPEN%%RFCOMM_CLOSE%%RFCOMM_OPEN%%RF
COMM_CLOSE%%DISCONN%%CONNECT,*MACIDofUSBBT*%%RFCOMM_OPEN%%RFCOMM_CLOSE% %RFCOMM_OPEN%%RFCOMM_CLOSE%%DISCONN% 
continuously.
 
I tried changing many settings of the module but couldn't find a solution.
 
I would be glad for any help.
 
 
 
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5