• AVR Freaks

Hot!Clock generation

Author
B.Kaavya
New Member
  • Total Posts : 5
  • Reward points : 0
  • Joined: 2019/09/02 23:51:17
  • Location: 0
  • Status: offline
2019/09/05 22:27:30 (permalink)
0

Clock generation

Hi,
I am using ATSAMD10C14 MCU ,
trying to use MDC and MDIO protocal for communication between MCU and transceiver.
Transceiver part no. DP83869HMRGZT
Here my issue is that am unable to generate internal clock more than 2.5MHz whereas am providing  8MHz  for internal clock configuration and it is getting divided while getting the output .
 
Can you please provide me solution for how to generate clock frequency more than 2.5 MHz.
 
Thanks and Regards,
Kaavya.
#1

1 Reply Related Threads

    QuiqueG
    Super Member
    • Total Posts : 122
    • Reward points : 0
    • Joined: 2010/09/01 12:35:40
    • Location: DM43BH
    • Status: offline
    Re: Clock generation 2019/09/09 10:15:48 (permalink)
    0
    Hello Kaavya:
     
       Most of the users in this forum are experienced in PIC microcontroller devices.
      This question will be better answered in AVRfreaks forum; since there is where most of the AVR experienced users reside.
     
    https://www.avrfreaks.net/search/site/ATSAMD10C14?solrsort=ds_created%20desc
       
      And...  when you post a question make sure to share your source code. This will help other users make recommendations and determine where the problem is.
     
    Thanks
     
    post edited by DeutcheN - 2019/09/09 10:19:31
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5