• AVR Freaks

Hot!Configurable stop bits on RN4678?

Author
daatkins
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2019/08/08 02:31:16
  • Location: 0
  • Status: offline
2019/09/04 06:19:00 (permalink)
0

Configurable stop bits on RN4678?

Hi everyone,
I’m trying to replace a wired Modbus interface with Bluetooth. The problem I have is that Modbus specifies two stop bits, whereas it looks like the RN4678’s UART is fixed at one.
 
Are there any hidden configuration commands or other easy ways around this problem?
 
Regards,
David.
 
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5