• AVR Freaks

Hot!Harmony 3 I2c Slave support?

Author
Volker
Super Member
  • Total Posts : 172
  • Reward points : 0
  • Joined: 2007/01/29 03:00:06
  • Location: Germany
  • Status: offline
2019/09/04 03:58:38 (permalink)
0

Harmony 3 I2c Slave support?

Hi,
 
i want to use an i2c slave with a same54 xpro board but in harmony i can only select i2c master.
 
is there no support for an i2c slave in harmony 3?
Thanks.
#1

4 Replies Related Threads

    Volker
    Super Member
    • Total Posts : 172
    • Reward points : 0
    • Joined: 2007/01/29 03:00:06
    • Location: Germany
    • Status: offline
    Re: Harmony 3 I2c Slave support? 2019/09/08 22:42:06 (permalink)
    0
    Hello,
     
    has no one use an i2c slave with harmony 3 yet?
    #2
    marelcom
    New Member
    • Total Posts : 19
    • Reward points : 0
    • Joined: 2018/01/17 03:18:47
    • Location: 0
    • Status: offline
    Re: Harmony 3 I2c Slave support? 2019/09/10 04:26:40 (permalink)
    0
    Hi

    I think harmony v3 is still not finished yet.
    I tried to configurate i2c slave with harmony v3 as well, but i couldn't find any option to set the slave options :-(
     
    regards
    Markus
    #3
    Volker
    Super Member
    • Total Posts : 172
    • Reward points : 0
    • Joined: 2007/01/29 03:00:06
    • Location: Germany
    • Status: offline
    Re: Harmony 3 I2c Slave support? 2019/09/11 22:38:17 (permalink)
    0
    Hi,
     
    i have the information that the i2c slave would be implemented late October...
     
    Regards
    Volker
    #4
    ric
    Super Member
    • Total Posts : 23596
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: Harmony 3 I2c Slave support? 2019/09/11 22:41:20 (permalink)
    0
    Which year? ;)
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #5
    Jump to:
    © 2019 APG vNext Commercial Version 4.5