• AVR Freaks

Hot!Removing 'logical' folder (Important Files, Header Files) from a project

Author
nyholku
Junior Member
  • Total Posts : 120
  • Reward points : 0
  • Joined: 2008/04/30 05:13:58
  • Location: 0
  • Status: offline
2019/08/30 00:17:11 (permalink)
0

Removing 'logical' folder (Important Files, Header Files) from a project

Hi, I find the 'logical' folders (for example 'Important Files')in MPLAB X  to be abominations.
 
How can I get rid of them?
 
wbr Kusti
 
#1

7 Replies Related Threads

    Gort2015
    Klaatu Barada Nikto
    • Total Posts : 3936
    • Reward points : 0
    • Joined: 2015/04/30 10:49:57
    • Location: 0
    • Status: offline
    Re: Removing 'logical' folder (Important Files, Header Files) from a project 2019/08/30 02:25:05 (permalink)
    0
    Abominations! that's a bit extreme.
     
    Delete the important files, it's what they are there for.

    MPLab X playing up, bug in your code? Nevermind, Star Trek:Discovery will be with us soon.
    https://www.youtube.com/watch?v=Iu1qa8N2ID0
    + ST:Continues, "What Ships are Made for", Q's back.
    #2
    nyholku
    Junior Member
    • Total Posts : 120
    • Reward points : 0
    • Joined: 2008/04/30 05:13:58
    • Location: 0
    • Status: offline
    Re: Removing 'logical' folder (Important Files, Header Files) from a project 2019/08/30 03:59:45 (permalink)
    0
    Sorry I did not make myself understood. 
     
    I want to get rid of the folder, not the files.
    On file system I have:
    projectx/Makefile
    on the IDE this is displayed as
    Important Files/Makefile
    and I want to get rid of the 'Important Files' and not the Makefile.
     
     
    For the record, I have no UN-important files in my project as I try to keep everything tidy,
    so I think it is an abomination to have folder named like that. The IDE should not dictate
    how my project is organised and neither should it try show a false facade of how the 
    project is organised.
     
    I'm not a kid anymore (approaching 60 after a career of 40 years in embedded programming)
    I don't need handholding and making things look simple and pretty, I want to see things as
    they are and be in control.
     
    wbr Kusti
     
    #3
    crosland
    Super Member
    • Total Posts : 1979
    • Reward points : 0
    • Joined: 2005/05/10 10:55:05
    • Location: Warks, UK
    • Status: offline
    Re: Removing 'logical' folder (Important Files, Header Files) from a project 2019/08/30 06:06:09 (permalink)
    0
    nyholku
    I'm not a kid anymore (approaching 60 after a career of 40 years in embedded programming)
    I don't need handholding and making things look simple and pretty, I want to see things as
    they are and be in control.

     
    I sympathise :) I think using logical folders has a lot to do with the way NetBeans works.
    #4
    rodims
    Super Member
    • Total Posts : 1557
    • Reward points : 0
    • Joined: 2009/02/10 11:08:59
    • Location: 51.9627, 7.6262
    • Status: offline
    Re: Removing 'logical' folder (Important Files, Header Files) from a project 2019/08/30 07:10:33 (permalink)
    0
    I want to see things as they are and be in control.

    If you like that, then why you don't edit configurations.xml ?
    #5
    Gort2015
    Klaatu Barada Nikto
    • Total Posts : 3936
    • Reward points : 0
    • Joined: 2015/04/30 10:49:57
    • Location: 0
    • Status: offline
    Re: Removing 'logical' folder (Important Files, Header Files) from a project 2019/08/30 07:16:31 (permalink)
    0
    I would also prefer o/s (shortcuts to folders) so that when you rename/add/move a file or folder, it get's done in the o/s not some front end that is not reliable.
     
    MPLab X on VS should have been there from day one as a plugin.
     
    It's not very smart either:
    The option is there to rename a library, it fails on that (breaks the tree and linkage), the library has to be removed, renamed and then added again.

    MPLab X playing up, bug in your code? Nevermind, Star Trek:Discovery will be with us soon.
    https://www.youtube.com/watch?v=Iu1qa8N2ID0
    + ST:Continues, "What Ships are Made for", Q's back.
    #6
    nyholku
    Junior Member
    • Total Posts : 120
    • Reward points : 0
    • Joined: 2008/04/30 05:13:58
    • Location: 0
    • Status: offline
    Re: Removing 'logical' folder (Important Files, Header Files) from a project 2019/08/30 20:28:17 (permalink)
    0
    @rodims, thanks! Good idea. At first it seemed like this would be solution. Then I removed all the folders and the project would not load. Next I tried leaving just one folder and all the folders came back when I opened the project even though they are not in the xml file. Hmm, maybe made a mistake somewhere I will try again.
     
    @crossland, yeah, Netbeans, what a pitty when so many other semiconductor companies have chosen Eclipse Microchip went with Netbeans. Hmm, here is a thought: since basically I don't need or like anything that Netbeans offers I should be able to use Eclipse if I can only use the debug/loader from command line to program my chips.
    This needs investigation. :) 
     
    #7
    moser
    Super Member
    • Total Posts : 568
    • Reward points : 0
    • Joined: 2015/06/16 02:53:47
    • Location: Germany
    • Status: offline
    Re: Removing 'logical' folder (Important Files, Header Files) from a project 2019/09/02 04:24:36 (permalink)
    0
    Maybe this is something for you:
    https://microchipdeveloper.com/mplabx:work-outside
    #8
    Jump to:
    © 2020 APG vNext Commercial Version 4.5