• AVR Freaks

Hot!dsPIC33EP512MU810 uart pins

Author
fluxanode
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2017/04/03 11:04:35
  • Location: 0
  • Status: offline
2019/08/28 16:24:27 (permalink)
0

dsPIC33EP512MU810 uart pins

Can someone please tell me what pin numbers on the dsPIC33EP512MU810 IC are the pin to use for U1, U2, U3, and U4 UART's?
and tell me where you found that info?  i don't see it in the data sheet.
#1

3 Replies Related Threads

    du00000001
    Just Some Member
    • Total Posts : 3348
    • Reward points : 0
    • Joined: 2016/05/03 13:52:42
    • Location: Germany
    • Status: offline
    Re: dsPIC33EP512MU810 uart pins 2019/08/29 14:17:08 (permalink)
    0
    (I didn't even look into the datasheet, so no references...)
    If it's got that many UARTs, some if not all have their I/O pins assigned via the PPS configuration registers. So look into the chapters U(S)ART and PPS.

    PEBKAC / EBKAC / POBCAK / PICNIC (eventually see en.wikipedia.org)
    #2
    nice
    Super Member
    • Total Posts : 1090
    • Reward points : 0
    • Joined: 2004/09/18 11:42:25
    • Location: Germany
    • Status: offline
    Re: dsPIC33EP512MU810 uart pins 2019/08/29 15:01:50 (permalink)
    0
    du00000001
    If it's got that many UARTs

     
    Yes, it does.
     
    du00000001
    some if not all have their I/O pins assigned via the PPS configuration registers.


    All is the corect answer. wink: wink
    I'm not aware of any 16-bit PIC with PPS having dedicatd pins for any of its UARTs.
    #3
    ric
    Super Member
    • Total Posts : 25562
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: dsPIC33EP512MU810 uart pins 2019/08/29 15:11:59 (permalink)
    4 (1)
    Latest datasheet is at http://ww1.microchip.com/...n/DeviceDoc/70616g.pdf
    Page 26 tells you U1TX, U1RX etc are all assigned by PPS
    http://ww1.microchip.com/...Doc/70616g.pdf#page=26
     
    Section "11.4 Peripheral Pin Select" introduces PPS
    http://ww1.microchip.com/...oc/70616g.pdf#page=210
     
     The registers for mapping inputs U1RX to U4RX are in the table on pages 211-212 and the values to put into them for each pin are in the table on pages 231-214
     
    The output mappings for U1TX to U4TX are on pages 215-216
     
    Read this chapter carefully. It is a great facility once you get your head around it.

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5