• AVR Freaks

Hot!Can not debug project

Author
rafalk
New Member
  • Total Posts : 5
  • Reward points : 0
  • Joined: 2013/03/08 17:49:20
  • Location: 0
  • Status: offline
2019/08/28 15:45:47 (permalink)
0

Can not debug project

I came back to a legacy project that was set aside for a few months. No changes were in the project made since that point in time. The project was working fine at that point in time. When I ran the debugger it would indicate Target Halted, although no debug set point was indicated. After several seconds the message "A communication error with the debug tool has occurred. The tool will attempt to recover momentarily." appears. This problem was not there the last time this project was run and no changes were made to the project. Note that this is a legacy project running under the C32 compiler. Diagnostics performed include:
 
 
* Changed to a different PICkit4 debug tool.
* Tried debugging with a similar legacy project - all worked fine - so this seems not to be a hardware issue.
* Took project to a different computer, uC hardware and debugger - same results
* Checked configuration bits - all settings the same as similar legacy project
* Tried to rebuild the project, but apparently MPLAB X IDE will not allow selection of the C32 compiler for PIC32 uC.
 
I looked in the forums and found nothing on this issue. Could really use some help here.
 
Thanks, Aaron
#1

4 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 18779
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: Can not debug project 2019/08/28 16:05:58 (permalink)
    0
    You can use C32. If you install it first
    #2
    rafalk
    New Member
    • Total Posts : 5
    • Reward points : 0
    • Joined: 2013/03/08 17:49:20
    • Location: 0
    • Status: offline
    Re: Can not debug project 2019/08/28 16:10:14 (permalink)
    0
    C32 is already installed. MPLAB X will not allow selection of C32 compiler for PIC32MX chips
    #3
    Jim Nickerson
    User 452
    • Total Posts : 6682
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Re: Can not debug project 2019/08/29 06:38:08 (permalink)
    +1 (1)
    Seems to work for me
    Attachments are not available: Download requirements not met

    Attachment(s)

    Attachments are not available: Download requirements not met
    #4
    skeev
    New Member
    • Total Posts : 15
    • Reward points : 0
    • Joined: 2018/11/08 10:27:03
    • Location: 0
    • Status: offline
    Re: Can not debug project 2019/08/29 16:01:44 (permalink)
    0
    Any chance a license expired or was for a different platform?
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5