• AVR Freaks

Hot!Explorer 16/32 Development Board

Author
FrankV2
New Users
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2019/08/23 10:09:54
  • Location: 0
  • Status: offline
2019/08/27 01:51:51 (permalink)
0

Explorer 16/32 Development Board

Good morning everyone,
I’m implementing an experiment with the Explorer 16/32 development board on which I need to install the LoRa RF Click module (https://www.mikroe.com/lora-rf-click).
More precisely, I need the instructions (code) for enabling the PINs that allow the Explorer mikroBUS A to work.
I’m currently referring to the GitHub code https://github.com/MikroE.../mikroBUS%20API/dsPIC.
Thank you all for your help.
Best Regards,
Frank
#1

1 Reply Related Threads

    DeutscheN
    Super Member
    • Total Posts : 122
    • Reward points : 0
    • Joined: 2010/09/01 12:35:40
    • Location: DM43BH
    • Status: offline
    Re: Explorer 16/32 Development Board 2019/09/03 14:51:27 (permalink)
    0
      Try using MCC.
     
     Under Device Resources there is an example of LoRa RF click which enables you to get up and going.
     
     
     
     
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5