• AVR Freaks

Hot!One RN4871 in central client role with multiple connected peripherals? Is it possible?

Author
vito.incallito
New Member
  • Total Posts : 5
  • Reward points : 0
  • Joined: 2003/11/07 12:44:03
  • Status: offline
2019/08/26 07:30:03 (permalink)
0

One RN4871 in central client role with multiple connected peripherals? Is it possible?

Hello I would like to have a RN4871 in Central (client) mode, which receives continuous updates via Indications/Notifications from about 10 RN4871 configured as Peripheral (Server) nodes.
I have read the documentation but it seems to me that the RN4871, also in Client mode, can be connected only to a single Server at once.
So my intent is impossible? Or, if it is possible, is there any example on how to do it?
Thank you.
--VM.
 
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5