• AVR Freaks

Hot!CAN Controllers compatibility

Author
antesther
New Member
  • Total Posts : 21
  • Reward points : 0
  • Joined: 2019/06/04 09:44:13
  • Location: 0
  • Status: offline
2019/08/23 06:11:22 (permalink)
0

CAN Controllers compatibility

Hello All,
 
I recently built a CAN bus with six nodes (PIC18F2580) with ECAN modules (Enhanced Controller Area Network) plus 6 CAN Transceivers (MCP2561), and I got a NXP Development Board (FRDM-KE06Z) with CAN communication enabled called MSCAN (Motorola Scalable Controller Area Network)... I was able to communicate two of this development boards, but when i try to hook up one of them to the pics CAN bus i just can't receive any message.
 
Could it be that using different CAN controllers (One ECAN and other MSCAN) is the reason why it does not receive any message?
#1

1 Reply Related Threads

    crosland
    Super Member
    • Total Posts : 1777
    • Reward points : 0
    • Joined: 2005/05/10 10:55:05
    • Location: Warks, UK
    • Status: offline
    Re: CAN Controllers compatibility 2019/08/23 08:29:52 (permalink)
    0
    No. 
     
    Most likely incorrect settings for the bit rate, etc., or incorrect protocol being used for the messages.
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5