• AVR Freaks

Hot!PICKIT4 Error: Target Device ID (0x2000) is an Invalid Device ID.

Author
Fausti
New Member
  • Total Posts : 19
  • Reward points : 0
  • Joined: 2014/11/23 11:59:51
  • Location: Germany
  • Status: offline
2019/08/22 01:57:26 (permalink)
0

PICKIT4 Error: Target Device ID (0x2000) is an Invalid Device ID.

Hello, my configuration is:
PICKIT4, PIC18F46K20, Target board Pin 2 and 6 not connected.
Project setting: Power target from PK4 = On
 
When programming a device, following meassage will appear: 
Target Device ID (0x2000) is an Invalid Device ID. Please check your connections to the Target Device.
 
But programming is sucessfull.
With PK3 same settings this fault message will not appear.
#1

3 Replies Related Threads

    ric
    Super Member
    • Total Posts : 25483
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: offline
    Re: PICKIT4 Error: Target Device ID (0x2000) is an Invalid Device ID. 2019/08/22 02:02:35 (permalink)
    0
    Why is pin#2 not connected? The programmer REQUIRES that pin to set the voltage transition levels.
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    Fausti
    New Member
    • Total Posts : 19
    • Reward points : 0
    • Joined: 2014/11/23 11:59:51
    • Location: Germany
    • Status: offline
    Re: PICKIT4 Error: Target Device ID (0x2000) is an Invalid Device ID. 2019/08/22 02:06:11 (permalink)
    0
    PICKIT3 is working perfect without Pin 2 connected.
    #3
    ric
    Super Member
    • Total Posts : 25483
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: offline
    Re: PICKIT4 Error: Target Device ID (0x2000) is an Invalid Device ID. 2019/08/22 02:07:16 (permalink)
    5 (1)
    You're probably using the dodgy workaround of telling the PK3 to supply power, so it sets the Vdd voltage itself.
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5