• AVR Freaks

Hot!The program file could not be loaded: Invalid file offset requested

Author
skeev
New Member
  • Total Posts : 15
  • Reward points : 0
  • Joined: 2018/11/08 10:27:03
  • Location: 0
  • Status: offline
2019/08/21 14:30:00 (permalink)
0

The program file could not be loaded: Invalid file offset requested

Though struggling mightily,
I've yet to be able to use a debugger with MPLAB X v5.05 .
Usually, if I try to make a debugging build, MPLAB complains
"The program file could not be loaded: Invalid file offset requested".
One time it had a lot of complaints about Buttons.i .
After removing all the .i files and trying again,
I got the quoted message.
 
Searching brought me to the suggestion
that I should update to at least 2.3.0 .
Not a real help.
An alternative suggestion was to use coff instead of elf.
No idea how.
 
How do I debug with MPLAB X?
If I need coff, how do I do that?
#1

2 Replies Related Threads

    ric
    Super Member
    • Total Posts : 25576
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: The program file could not be loaded: Invalid file offset requested 2019/08/22 13:19:59 (permalink)
    0
    What device family/PIC model are you compiling for?
     

    If I need coff, how do I do that?

    You would change a setting in the project properties. Top left icon on the project toolbar.

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    skeev
    New Member
    • Total Posts : 15
    • Reward points : 0
    • Joined: 2018/11/08 10:27:03
    • Location: 0
    • Status: offline
    Re: The program file could not be loaded: Invalid file offset requested 2019/08/22 14:15:31 (permalink)
    0
    I've got a PIC32MX795F512L.
     
    I can find properties ok,
    but the bit that lets me change from elf to coff eludes me.
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5