• AVR Freaks

Hot!RN4870 Remote Command

Author
CatLuigi
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2019/08/18 04:50:29
  • Location: 0
  • Status: offline
2019/08/20 08:37:47 (permalink)
0

RN4870 Remote Command

I can't get into the remote command mode.
When I write the command "!,1" it gives me ERR.
The required conditions are met:
  • Both local and remote devices support UART Transparent feature.
  • The two devices are already connected and secured.
  • The BLE link between devices are secured.
What I don't understand is that:
  • The first 4 bytes of local fixed PIN code match those of the peer device.
How do I know the pin of the local device?
I did the tests with a RN4870 module connected to the PC and an Android smartphone.
Thank you.
#1

2 Replies Related Threads

    myZigbee
    Super Member
    • Total Posts : 245
    • Reward points : 0
    • Joined: 2006/11/17 08:34:52
    • Location: 0
    • Status: offline
    Re: RN4870 Remote Command 2019/08/22 13:41:08 (permalink)
    5 (1)
    The remote command feature in RN487x only supports connection between each other. If you set the same pin with command "SP" on both devices, then you should be able to enable the remote command feature.
     
    #2
    CatLuigi
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2019/08/18 04:50:29
    • Location: 0
    • Status: offline
    Re: RN4870 Remote Command 2019/08/23 02:43:40 (permalink)
    0
    Ok thanks for the reply, now it's all clear.
    Too bad that you can't control directly with your smartphone.
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5