• AVR Freaks

Hot!PICKit 3 works fine with PICKIT 3 v3.10 but not with MPLAB

Author
Jan Lichtenbelt
New Member
  • Total Posts : 15
  • Reward points : 0
  • Joined: 2016/12/15 08:45:58
  • Location: 0
  • Status: offline
2019/08/19 04:25:08 (permalink)
0

PICKit 3 works fine with PICKIT 3 v3.10 but not with MPLAB

I have one PC and one laptop, both Window 10, 64 bits.
I installed MPLAB IPE v5.25 on both and the older software Pickit 3 v3.10 on the laptop.
Programming my PIC16F1847 is correctly done with the Pickit 3 v3.10 software. However, on the same laptop MPLAB X IPE does see the PICKIT 3 at all?????
On the PC, the MPLAB IPE sees the PicKit 3 tool, but power target circuit from PM3 does not power the microchip. And loading the hex file into the microchip resulted in the message the target must be powered externally. But neither power from the Pickit 3 tool, neither from external power help to down load the hex file. It fails.
In all cases I used MPLAB as administrator.
 
What can I do?
 
Kind regards
 
Jan (John) Lichtenbelt
#1

11 Replies Related Threads

    vkalyan
    New Member
    • Total Posts : 27
    • Reward points : 0
    • Joined: 2016/02/15 22:26:47
    • Location: 0
    • Status: offline
    Re: PICKit 3 works fine with PICKIT 3 v3.10 but not with MPLAB 2019/08/19 09:22:36 (permalink)
    0
    Hi Jan,
     
    On the laptop I think you need to use the driver switcher tool in order for the latest version of IPE to identify PK3. This is located under C:\Program Files (x86)\Microchip\MPLABX\v5.25\Switcher\64Bit
     
    Regarding the issue of powering the target from the tool, what I usually follow is I go to the Power Settings tab first, select the checkbox (Power target from tool), come back to Operate tab and then 'Connect' to the tool. This way the tool will attempt to provide the supply and if it fails you'll obviously see an error. Most of the times I see 'Target Device ID mismatch error' kind of message. In my case I sometimes get my connections wrong or I put my board's jumper on the wrong supply pin. So I'm interested to see what is the error message that you are seeing. Can you post a snapshot of it?
    #2
    Jerry Messina
    Super Member
    • Total Posts : 451
    • Reward points : 0
    • Joined: 2003/11/07 12:35:12
    • Status: offline
    Re: PICKit 3 works fine with PICKIT 3 v3.10 but not with MPLAB 2019/08/19 10:06:41 (permalink)
    0
    You don't need the driver switcher with the PK3. It won't do anything.
     
    If you're going back and forth between the old Pickit3 software and MPLABX you should make sure that the PK3 gets its firmware reprogrammed whenever you switch apps.
     
    #3
    vkalyan
    New Member
    • Total Posts : 27
    • Reward points : 0
    • Joined: 2016/02/15 22:26:47
    • Location: 0
    • Status: offline
    Re: PICKit 3 works fine with PICKIT 3 v3.10 but not with MPLAB 2019/08/19 10:21:59 (permalink)
    0
    However, on the same laptop MPLAB X IPE does see the PICKIT 3 at all?????

     
    This means that the tool is not showning up in the dropdown of IPE at all. The reason is that the MPLAB USB comm has been set to work with older software and MPLAB X IPE doesn't read the tool. When the driver is switched back to work with MPLABX, then the firmware upgrade will automatically happen if required.
    #4
    Jan Lichtenbelt
    New Member
    • Total Posts : 15
    • Reward points : 0
    • Joined: 2016/12/15 08:45:58
    • Location: 0
    • Status: offline
    Re: PICKit 3 works fine with PICKIT 3 v3.10 but not with MPLAB 2019/08/19 11:07:01 (permalink)
    0
    Hi vkalyan and Jerry
     
    I'm happy that you help me to solve the problem.
    1) I tried the both switchers (ICD3_switcher64.bat and RI_switcher64.bat as administrator), without success.
    2) I tried the PICKIT 3 with software version 3.10, which works well, see picture.
    3) I tried MAPLAB IDE V5.25 without success. I set the power off and on the chip in the software, but in practise the 5V is in both cases available on the microchip. But, as you see in the picture, this software does not see the PICKIT 3. I cannot select any tool.
     
    Kind regards
     
    Jan
     
    PS. I intended to add the pictures, but I don't know how?
    #5
    Jan Lichtenbelt
    New Member
    • Total Posts : 15
    • Reward points : 0
    • Joined: 2016/12/15 08:45:58
    • Location: 0
    • Status: offline
    Re: PICKit 3 works fine with PICKIT 3 v3.10 but not with MPLAB 2019/08/19 11:37:27 (permalink)
    #6
    Jan Lichtenbelt
    New Member
    • Total Posts : 15
    • Reward points : 0
    • Joined: 2016/12/15 08:45:58
    • Location: 0
    • Status: offline
    Re: PICKit 3 works fine with PICKIT 3 v3.10 but not with MPLAB 2019/08/21 02:47:48 (permalink)
    0
    Who can help me with this serious problem?
     
    With kind regards
     
    Jan
     
     
    #7
    Les
    Super Member
    • Total Posts : 240
    • Reward points : 0
    • Joined: 2011/02/23 04:27:28
    • Location: UK
    • Status: offline
    Re: PICKit 3 works fine with PICKIT 3 v3.10 but not with MPLAB 2019/08/21 04:21:35 (permalink)
    0
    I seem to remember a option to switch PK3 between MPLAB  and stand alone mode .. may be dreaming :) 
    #8
    ric
    Super Member
    • Total Posts : 25127
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: PICKit 3 works fine with PICKIT 3 v3.10 but not with MPLAB 2019/08/21 05:32:43 (permalink)
    0
    -deleted

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #9
    Jim Nickerson
    User 452
    • Total Posts : 6414
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Re: PICKit 3 works fine with PICKIT 3 v3.10 but not with MPLAB 2019/08/21 06:05:46 (permalink)
    0
    Maybe you could ask support http://support.microchip.com
    #10
    Jan Lichtenbelt
    New Member
    • Total Posts : 15
    • Reward points : 0
    • Joined: 2016/12/15 08:45:58
    • Location: 0
    • Status: offline
    Re: PICKit 3 works fine with PICKIT 3 v3.10 but not with MPLAB 2019/08/21 06:16:13 (permalink)
    0
    Dear Les,
     
    Tell me how I can switch between PK3 and MPLAB?
     
    Kind regrads
     
    Jan
    #11
    Les
    Super Member
    • Total Posts : 240
    • Reward points : 0
    • Joined: 2011/02/23 04:27:28
    • Location: UK
    • Status: offline
    Re: PICKit 3 works fine with PICKIT 3 v3.10 but not with MPLAB 2019/08/21 06:36:42 (permalink)
    0
    Jan... I am sure i saw it somewhere ... but cannot find it, I was using the PK3 standalone on a win 7 machine, a year ago but now switched to linux.mint so difficult to load / track / find .. not given up yet ! You could try forcing a reload of PK3  FW  with  MPLAB 8.xx ..  
    This my be what I remember ( see last post ! )
    https://www.microchip.com/forums/m1084860.aspx
    post edited by Les - 2019/08/21 06:44:32
    #12
    Jump to:
    © 2020 APG vNext Commercial Version 4.5