• AVR Freaks

Hot!MPLAB XC8 v2.10 Released - nearly

Author
rjc101
Super Member
  • Total Posts : 113
  • Reward points : 0
  • Joined: 2016/07/08 14:56:34
  • Location: 0
  • Status: online
2019/08/18 12:19:39 (permalink)
0

MPLAB XC8 v2.10 Released - nearly

The link to the MacOS version still points to v2.05, the others seems OK.  If I try and grab the file directly with the url below it isn't found.
http://ww1.microchip.com/downloads/en/DeviceDoc/xc8-v2.10-full-install-osx-installer.dmg

post edited by rjc101 - 2019/08/18 12:23:22
#1

3 Replies Related Threads

    mad_c
    Super Member
    • Total Posts : 1209
    • Reward points : 0
    • Joined: 2010/12/12 17:48:27
    • Location: Brisbane, Australia
    • Status: offline
    Re: MPLAB XC8 v2.10 Released - nearly 2019/08/18 14:32:42 (permalink)
    +1 (1)
    Hi,
     
    I'll send a note to the relevant people just to check that the correct image was uploaded. The DAM that controls all this is very temperamental, and it might just be having a slow Sunday.
     
    Jeff.
     
    #2
    digisign
    Starting Member
    • Total Posts : 32
    • Reward points : 0
    • Joined: 2010/09/02 15:01:26
    • Location: Stockholm , Sweden
    • Status: offline
    Re: MPLAB XC8 v2.10 Released - nearly 2019/08/18 23:44:53 (permalink)
    -1 (1)
    The link does not work !!
    #3
    rjc101
    Super Member
    • Total Posts : 113
    • Reward points : 0
    • Joined: 2016/07/08 14:56:34
    • Location: 0
    • Status: online
    Re: MPLAB XC8 v2.10 Released - nearly 2019/08/18 23:51:50 (permalink)
    0
    digisign
    The link does not work !!

    That’s the problem, the file isn’t there. Looks like it will get sorted pretty quickly.
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5