• AVR Freaks

Hot!How to get 60 days PRO license (XC8)

Author
newbie_pic
Starting Member
  • Total Posts : 31
  • Reward points : 0
  • Joined: 2019/07/05 19:39:30
  • Location: India
  • Status: offline
2019/08/14 20:59:47 (permalink)
0

How to get 60 days PRO license (XC8)

Hi, when I set Optimization in XC8 to 3 or s I got this warning - Compiler option (Optimization level > 2) ignored because this feature requires the MPLAB XC8 PRO compiler. And I get to know that there is 60 day PRO license available. How to get that?
#1

2 Replies Related Threads

    ric
    Super Member
    • Total Posts : 25116
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: How to get 60 days PRO license (XC8) 2019/08/14 21:14:03 (permalink)
    +1 (1)
    You are asked if you want to activate it when you install XC8, so just do a re-install.
    n.b. you can only do this once.
    There is also a monthly rental available.
     
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    newbie_pic
    Starting Member
    • Total Posts : 31
    • Reward points : 0
    • Joined: 2019/07/05 19:39:30
    • Location: India
    • Status: offline
    Re: How to get 60 days PRO license (XC8) 2019/08/14 21:21:38 (permalink)
    0
    Yes I got a window after installing XC8 saying Click here to get free, 60 day evaluation of PRO as a link but when I pressed that it does nothing. I waited for some time and then I pressed Next >. What to do now?
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5