• AVR Freaks

PIC32MX wrong bootloader

Author
P.Milchev
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2019/07/30 01:37:21
  • Location: 0
  • Status: offline
2019/08/14 08:44:00 (permalink)
0

PIC32MX wrong bootloader

Hello everyone,
 
My name is Petar Milchev and I am working with PIC32MX575F512L processor. 
Unfortunately I upload wrong bootloader (for PIC32MX470F512L) on that chip and now I can't access it.
When I try to connect with MPLAB IPE, it said:
"...
Target voltage detected
Unable to connect to the target device.
Failed to get Device ID"
 
Does anyone have some ideas?
Is there any force boot, or something similar, which will help me to erase the chip and upload the right bootloader?
 
Thanks and Regards,
Petar
#1

4 Replies Related Threads

    ric
    Super Member
    • Total Posts : 29504
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: PIC32MX wrong bootloader 2019/08/14 20:26:19 (permalink)
    0
    What board is your PIC on?
    A Microchip evaluation board, or something you designed?
     
    What programmer are you using?
    How is it connected to the PIC?
     
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    P.Milchev
    New Member
    • Total Posts : 3
    • Reward points : 0
    • Joined: 2019/07/30 01:37:21
    • Location: 0
    • Status: offline
    Re: PIC32MX wrong bootloader 2019/08/14 23:37:51 (permalink)
    0
    Hello Ric,
     
    Thank you for the quick response.
    I am using PIC on a custom board. Its used for controlling an audio multimedia.
    We are using PicKit3 for debugging and programming. It is connected throw its serial programming port.
     
    I am wondering, could it be dead? Before I upload the wrong bootloader, it works fine.
    Also I think that two MCUs could be replaced. I mean, that they share almost same pinout, so it couldn't be burned?
     
    So any ideas?
    #3
    maxruben
    Super Member
    • Total Posts : 3397
    • Reward points : 0
    • Joined: 2011/02/22 03:35:11
    • Location: Sweden
    • Status: offline
    Re: PIC32MX wrong bootloader 2019/08/15 10:44:52 (permalink)
    5 (1)
    Even with the wrong boot loader (or any program) you should be able to erase all.
     
    /Ruben
    #4
    P.Milchev
    New Member
    • Total Posts : 3
    • Reward points : 0
    • Joined: 2019/07/30 01:37:21
    • Location: 0
    • Status: offline
    Re: PIC32MX wrong bootloader 2019/08/19 03:33:10 (permalink)
    0
    Hello Ruben,
     
    I also think on that way...
    Well obviously I should replace the MCU with new one.
    Thank you
     
    Regards,
    Petar
    #5
    Jump to:
    © 2021 APG vNext Commercial Version 4.5