• AVR Freaks

Hot!using "generic" graphics controller

Author
TTBiker
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2019/08/07 20:55:20
  • Location: 0
  • Status: offline
2019/08/13 21:28:51 (permalink)
0

using "generic" graphics controller

Hello everyone. Hopefully someone has some information to get this working. I created a project with Harmony V2 and made a simple UI with graphics composer. I selected the generic display controller, and implemented functions to work with my driver. I have tested the driver without Harmony and it works perfectly. The problem is with harmony the display will initialize, but no image data will be sent to it. 
Basically I need to know if there is a list of requirements to get it working? Such as what functions in the generic controller need to be implemented, and what can just use the default implementations. For now I am not implementing any of the hardware accelerated aspects, I just want to get it displaying. 
using PIC32MK1024GPD064, ILI9341 240x320 display. The driver uses PMP. 
Any help would be great, thanks!!
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5