• AVR Freaks

Hot!Tag connect cables

Author
dbvanhorn
New Member
  • Total Posts : 20
  • Reward points : 0
  • Joined: 2019/08/13 07:03:40
  • Location: 0
  • Status: offline
2019/08/13 14:48:28 (permalink)
0

Tag connect cables

Does this unit use the same Tag-Connect cables as the Pickit-3?
#1

2 Replies Related Threads

    ric
    Super Member
    • Total Posts : 25116
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: Tag connect cables 2019/08/14 15:26:59 (permalink)
    0
    A PK4 has the same ICSP connector as a PK3, so if you have a Tag-Connect cable that fits a PK3 it should also work on the PK4.
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    dbvanhorn
    New Member
    • Total Posts : 20
    • Reward points : 0
    • Joined: 2019/08/13 07:03:40
    • Location: 0
    • Status: offline
    Re: Tag connect cables 2019/08/15 05:30:39 (permalink)
    0
    Ok, thanks!  I'm new to the whole Microchip ecosystem, just brought back those and other toys from Masters last week.
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5