• AVR Freaks

BM71 Power

Author
Burg
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2018/07/26 10:12:12
  • Location: 0
  • Status: offline
2019/08/12 12:48:30 (permalink)
0

BM71 Power

Greetings,
 
I am having an issue where my BM71 is still advertising even though the power through Vbat (PIN 14) is no longer on (removed). I'm not sure how it is still being powered on. It seems to have a voltage of around .6V on that pin at the time of advertising. Attached is an image of the schematic. Is it being powered through the Reset pin?
 
Thanks!

Attached Image(s)

#1

1 Reply Related Threads

    JustPlaneD
    New Member
    • Total Posts : 15
    • Reward points : 0
    • Joined: 2018/10/24 13:44:38
    • Location: 0
    • Status: offline
    Re: BM71 Power 2019/08/14 16:36:08 (permalink)
    0
    Check for current flow thru Rx and/or Tx. The device will attempt to power itself thru the body diodes if power is removed from Vbatt but there is voltage on any of the input pins.
    #2
    Jump to:
    © 2021 APG vNext Commercial Version 4.5