• AVR Freaks

Hot!How to get into simulator IDE V3.35 from my asm file

Author
microchipprob
Senior Member
  • Total Posts : 140
  • Reward points : 0
  • Joined: 2008/07/01 00:51:30
  • Location: 0
  • Status: offline
2019/08/12 06:20:44 (permalink)
0

How to get into simulator IDE V3.35 from my asm file

Freinds i have MPlabx ide v3.35 version in my pc, i have written some programs in Assembly langauge for (16F1828) device. The hardware is working well and in some portion of Hex to BCD i am finding a problem. Build is successful. I am unable to get into the simulator for step by step execution of that portion. Can anybody suggest as to how to get into the simulator for step by step execution of program. The menu at the IDE is confusing. I unable find help for simulator on internet or on you tube. Thanks for help in advance

B.J.Haricharan
#1

2 Replies Related Threads

    ric
    Super Member
    • Total Posts : 25116
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: offline
    Re: How to get into simulator IDE V3.35 from my asm file 2019/08/12 06:25:34 (permalink)
    +1 (1)
    In general, you would edit the project properties to select "Simulator" as the debugging tool, then start a debug session via the "Debug" menu.
    I'm just going on memory, as version 3.35 is so old. Why aren't you using the current version of MPLABX?
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    1and0
    Access is Denied
    • Total Posts : 10190
    • Reward points : 0
    • Joined: 2007/05/06 12:03:20
    • Location: Harry's Gray Matter
    • Status: offline
    Re: How to get into simulator IDE V3.35 from my asm file 2019/08/12 07:17:13 (permalink)
    0
    If you want to use an old IDE, you might be better off using the MPLAB v8.92.  At least it has better supports for assembly programs, and it does support your PIC device. ;)
     
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5