• AVR Freaks

Hot!Harmony v2.06 PIC32MK(GP) Board DUAL USB HOST

Author
lianna7
New Member
  • Total Posts : 5
  • Reward points : 0
  • Joined: 2019/07/19 07:04:34
  • Location: 0
  • Status: offline
2019/08/09 08:21:01 (permalink)
0

Harmony v2.06 PIC32MK(GP) Board DUAL USB HOST

Hello everyone,
 
i´m using the PIC32MK(GP) Board with the chip PIC32MK1024GPE100 for dual usb host with Harmony.
 
The attached picture is the Board top view.
 
Now I´m able to use one USB HOST with a usb hub on port 8. If I understand right, I can also use port 6 for the other USB. But I don´t know how can I configure it in Harmony? I have also attached the Harmony Configurator for USB in my present project. Even if I changed the parameter such as "Number of Devices" or "Number of CDC Host Driver Instances", the port 6 is still not working. 
 
Is there any document for my situation or has someone experience on it?
 
I´d appreciate any advice. Thanks in advance.
 
Na Lian

Attached Image(s)

#1

1 Reply Related Threads

    lianna7
    New Member
    • Total Posts : 5
    • Reward points : 0
    • Joined: 2019/07/19 07:04:34
    • Location: 0
    • Status: offline
    Re: Harmony v2.06 PIC32MK(GP) Board DUAL USB HOST 2019/08/12 01:25:07 (permalink)
    0
    I think I´ve found some information from the USB Harmony Help file.
     
    In page 249 it says "Along with Host Layer, the client drivers are designed to support multiple device of the same type (where multiple devices are connected to the host through a hub or is asingle device with multiple interfaces)." 
     
    So I understood before incorrect. 
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5