• AVR Freaks

Hot!Why is the "Copy framework files to local configuration directory" grayed out?

Author
m4l490n
Senior Member
  • Total Posts : 123
  • Reward points : 0
  • Joined: 2010/06/15 22:21:39
  • Location: 0
  • Status: offline
2019/08/08 16:48:36 (permalink)
0

Why is the "Copy framework files to local configuration directory" grayed out?

I'm trying to start a project with MHC2 and the "Copy framework files to local configuration directory" option is grayed out, my question is, why? What do I have to do to enable it?
 

Attached Image(s)

#1

1 Reply Related Threads

    _pawel_
    New Member
    • Total Posts : 5
    • Reward points : 0
    • Joined: 2019/09/16 05:57:36
    • Location: 0
    • Status: offline
    Re: Why is the "Copy framework files to local configuration directory" grayed out? 2019/09/21 22:22:06 (permalink)
    0
    This is the option you are looking for:

    Attached Image(s)

    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5