• AVR Freaks

Hot!RN4871 Command Mode

Author
teenix
Junior Member
  • Total Posts : 63
  • Reward points : 0
  • Joined: 2017/12/21 13:47:21
  • Location: Australia, Melbourne
  • Status: online
2019/08/07 17:51:17 (permalink)
0

RN4871 Command Mode

Hi
 
I am just starting to use the RN4781 module for a project.
 
From the data sheet, I know entering [$$$] via the serial port enters command mode.
 
However, in normal data mode, will the module enter command mode if it finds [$$$] buried somewhere in a data stream?
 
Is this what the  [SR] Command - "Command Mode Guard" bit is for, to disable this from happening?
 
cheers
 
Tony
#1

3 Replies Related Threads

    ric
    Super Member
    • Total Posts : 27975
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: RN4871 Command Mode 2019/08/07 19:24:01 (permalink)
    0
    teenix
    ...
    Is this what the  [SR] Command - "Command Mode Guard" bit is for, to disable this from happening?

    Yes. With that turned on, there must be one second of silence both before and after the "$$$" sequence.
    It is explained terribly in the user guide.
    http://ww1.microchip.com/...S50002466C.pdf#page=28

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    teenix
    Junior Member
    • Total Posts : 63
    • Reward points : 0
    • Joined: 2017/12/21 13:47:21
    • Location: Australia, Melbourne
    • Status: online
    Re: RN4871 Command Mode 2019/08/07 20:20:14 (permalink)
    0
    Hi,
     
    Thank you for prompt answer.
     
    One other problem which seems vague (to me), I assume the Bluetooth serial service also has to be started?
     
    This would be SS,40 (User Guide section: 2.4.22)
     
    cheers
     
    Tony
    #3
    JustPlaneD
    New Member
    • Total Posts : 15
    • Reward points : 0
    • Joined: 2018/10/24 13:44:38
    • Location: 0
    • Status: offline
    Re: RN4871 Command Mode 2019/08/14 16:23:42 (permalink)
    0
    Actually I believe Command Mode Guard requires 1 second before and after $$$ is received to switch the device into command mode __via_the_UART__. HOWEVER, If the SR,<hex16> (bit4 of the bitmap) is set to 0x2000 a HARDWARE pin must be pulled to send the into CommandMode.

    -I could be wrong but that's what DS50002466 2.4.21 seems to indicate
    And, yes you will have to enable the UART function with SS,40 or SS,OC (if you want UART+Device Information)
    post edited by JustPlaneD - 2019/08/14 16:26:38
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5