• AVR Freaks

AnsweredHot!Correct way to enable and handle Brownout Reset (BOR) in dsPIC33EP

Author
freddy7phil
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2019/07/10 01:16:38
  • Location: 0
  • Status: offline
2019/08/05 02:34:49 (permalink)
0

Correct way to enable and handle Brownout Reset (BOR) in dsPIC33EP

Hi all,
I was wondering how to enable and handle the Brownout Reset (BOR) in dsPIC33EP64MC504.
Is it enabled by default?
 
Cheers
Frederic
#1
ric
Super Member
  • Total Posts : 27015
  • Reward points : 0
  • Joined: 2003/11/07 12:41:26
  • Location: Australia, Melbourne
  • Status: online
Re: Correct way to enable and handle Brownout Reset (BOR) in dsPIC33EP 2019/08/05 02:42:33 (permalink) ☼ Best Answerby freddy7phil 2019/08/05 03:52:42
5 (2)
BOR is normally enabled in the CONFIG words in each device.
You don't have to "handle" it at all if you don't want to. If a brownout occurs, it will reset your device.
Only if you want to do something special straight after a brownout do you need any special handling.
 
 

I also post at: PicForum
Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
NEW USERS: Posting images, links and code - workaround for restrictions.
To get a useful answer, always state which PIC you are using!
#2
Jump to:
© 2020 APG vNext Commercial Version 4.5