• AVR Freaks

Harmony 2.06 Bootloader SD Card project for PIC32MK1024GPE100

Author
Kodl
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2003/11/07 12:47:06
  • Status: offline
2019/08/05 00:31:29 (permalink)
0

Harmony 2.06 Bootloader SD Card project for PIC32MK1024GPE100

Halo, I am  trying to create Harmony 2.06 Bootloader project for PIC32MK1024GPE100.
Harmony configuration (conf.png).
When I try to compile it, I get many link errors (err.png).
 
If I try to generate the same project for PIC32MZ1024EFG100 compilation is successful. Please, is there any chance to use PIC32MK1024GPE100 with Harmony SD card bootloader?

Attached Image(s)

#1

1 Reply Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 18850
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: Harmony 2.06 Bootloader SD Card project for PIC32MK1024GPE100 2019/08/05 06:19:06 (permalink)
    0
    It is complaining about not enough code space. Since you chip does have room, there is probably in error in the linker script.
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5