• AVR Freaks

Hot!AT91/SAMA5

Author
Jim Nickerson
User 452
  • Total Posts : 6688
  • Reward points : 0
  • Joined: 2003/11/07 12:35:10
  • Location: San Diego, CA
  • Status: online

4 Replies Related Threads

    ldesroches
    New Member
    • Total Posts : 1
    • Reward points : 0
    • Joined: 2019/08/04 23:43:09
    • Location: 0
    • Status: offline
    Re: AT91/SAMA5 2019/08/06 06:28:52 (permalink)
    0
    Yes, it is.
    #2
    moopau
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2019/11/27 02:21:17
    • Location: 0
    • Status: offline
    Re: AT91/SAMA5 2020/02/19 02:47:37 (permalink)
    0
    How much current is needed for the VDDFUSE power input ? specially the ATSAMA5D27C-LD1G
    #3
    scottoc
    New Member
    • Total Posts : 7
    • Reward points : 0
    • Joined: 2012/08/23 09:03:13
    • Location: 0
    • Status: offline
    Re: AT91/SAMA5 2020/03/05 08:01:47 (permalink)
    0
    According to the SAMA5D2 Discrete Power Supply Solution Application Note it is 50 mA.
     
    http://ww1.microchip.com/...n_Application-Note.pdf
     
     
    post edited by scottoc - 2020/03/05 08:03:45

    Attached Image(s)

    #4
    jtemples
    عُضْوٌ جَدِيد
    • Total Posts : 11894
    • Reward points : 0
    • Joined: 2004/02/13 12:31:19
    • Location: Southern California
    • Status: offline
    Re: AT91/SAMA5 2020/05/19 13:28:30 (permalink)
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5