• AVR Freaks

Hot!BM62 Blue tooth low energy disconnections

Author
Ali_king
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2018/10/30 07:09:00
  • Location: 0
  • Status: offline
2019/07/30 00:08:13 (permalink)
0

BM62 Blue tooth low energy disconnections

Hello,
 
I am experiencing disconnections from the BLE  after a random time period. I have been connecting to both apple and android phones.
the only thing i see before this disconnect happens are the commands : 
 
00 AA 00 04 32 00 00 00 CA 
00 AA 00 03 32 01 00 CA 
 
Has anyone got a fix or knows about this issue?
 
Best Regards,
Alister King 
#1

2 Replies Related Threads

    sayantapadar
    New Member
    • Total Posts : 3
    • Reward points : 0
    • Joined: 2019/07/23 21:48:34
    • Location: 0
    • Status: offline
    Re: BM62 Blue tooth low energy disconnections 2019/07/30 10:44:48 (permalink)
    0
    I have been facing the same issue. If you manage to solve it, please do write it here
    post edited by sayantapadar - 2019/07/31 08:37:09
    #2
    Luis Abós Luna
    New Member
    • Total Posts : 1
    • Reward points : 0
    • Joined: 2019/12/03 00:50:54
    • Location: 0
    • Status: offline
    Re: BM62 Blue tooth low energy disconnections 2019/12/04 06:56:21 (permalink)
    0
    I have exactly the same problem. We have a product that has two links: A2DP and BLE. We ALWAYS see the following:
    - when the connection sequence is 1st A2DP  and 2nd BLE no problem
    - when the connection sequence is 1st BLE and 2nd A2DP , if these connections are from different devices (2 different smatphones, or an smartphone and a PC), after a while, the connection is broken
     
    Tested in IOS and ANDROID, and it is the same.
     
    Any help fronm anyone?
     
    thanks
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5