• AVR Freaks

Hot!How to set up for PIC32MX370F512HT Bootloader with Harmony

Author
Guamstreet
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2018/11/06 13:40:48
  • Location: 0
  • Status: offline
2019/07/26 19:39:31 (permalink)
0

How to set up for PIC32MX370F512HT Bootloader with Harmony

Hi,all
I'm having So fun with pic16 or 18! and have made some DIY products!
So This time, I'd like to challenge PIC32MX370F512H with Bootloader! but I'm new to PIC32MX370F512H with Bootloader actually. What I want to get is how to generate the Bootloader in PIC32MX370F512H with Harmony. but I don't know that way well. So teach me that. That'll So Nice you give me about it directly, or even some reference sites!
Thanks in advance.
#1

4 Replies Related Threads

    iggardo
    Earthling
    • Total Posts : 30
    • Reward points : 0
    • Joined: 2013/07/13 07:03:47
    • Location: Earth
    • Status: offline
    Re: How to set up for PIC32MX370F512HT Bootloader with Harmony 2019/07/30 05:34:41 (permalink)
    0
    Hi.
    Which Harmony version are you using?
    Which bootloader type? USB, UART, Ethernet UDP?
     
    These short tutorials are for Harmony 2.03 and 2.06 but will work on other versions and other pic32 families with little changes.
    https://www.microchip.com...oad.axd?file=0;1003153
    https://ww1.microchip.com...ary%20Help%20v2.06.pdf
     
    Please search for Microchip application note AN1388
     
    Good starting point will be the examples from C:\HarmonyX_XX\apps\bootloader folder
     
    Good luck!
     
     
     
    #2
    Guamstreet
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2018/11/06 13:40:48
    • Location: 0
    • Status: offline
    Re: How to set up for PIC32MX370F512HT Bootloader with Harmony 2019/08/01 05:04:34 (permalink)
    0
    Thank you for your Great Chips! and So Sorry I get back to you Sooo late.
     
    I'm using the 2.06 version of Harmony and like to use the USB DEVICE.
     
    by the way, I have some question.
     
    What's AN1388 ?
     
    I've seen this much in the net when I search for about the Bootloader with Harmony.
     
    Is that the common Program for PIC32MX in Harmony? or Universal Program for all of PIC? I wonder?
     
    I'll be So happy you reply about this to me once more!
    #3
    iggardo
    Earthling
    • Total Posts : 30
    • Reward points : 0
    • Joined: 2013/07/13 07:03:47
    • Location: Earth
    • Status: offline
    Re: How to set up for PIC32MX370F512HT Bootloader with Harmony 2019/08/01 05:10:15 (permalink)
    0
    Guamstreet
    What's AN1388 ?



    This application note describes how to use bootloader to upgrade firmware on PIC32 devices without the need for an external programmer or debugger. The source code consists of following implementations of bootloader,
    1) UART
    2) USB device based on HID class
    3) USB host based on MSD class
    4) Ethernet
    5) SD card
     
    https://www.microchip.com....aspx?appnote=en554836

     
    #4
    Guamstreet
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2018/11/06 13:40:48
    • Location: 0
    • Status: offline
    Re: How to set up for PIC32MX370F512HT Bootloader with Harmony 2019/08/01 05:26:28 (permalink)
    0
    Thank you for your quick reply!
     
    OK! I got it!
     
    So I'll try the Great Chips that you gave me!
     
    ...but if I'll get some problem again in my Goal.
     
    May I post again?
     
    I'll be sooo happy you rescue memr green: mr green
     
    Anyway, I'll contact you when I get my Result ! 
     
    Thank you very much! 
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5