• AVR Freaks

Helpful ReplyHot!MCC configuration for the Explorer 16/32

Author
Vegas Mike
New Member
  • Total Posts : 17
  • Reward points : 0
  • Joined: 2006/11/16 09:27:24
  • Location: Las Vegas, Nevada, USA
  • Status: offline
2019/07/26 13:01:15 (permalink)
0

MCC configuration for the Explorer 16/32

Anyone prepared an MCC configuration for the Explorer 16/32?  Working on a demo project and using the Explorer 16/32 development board.  Would really help to have an MCC configuration file available so I don't need to reverse-engineer the Explorer 16/32 to set pin functions and appropriately set configuration bits.  These functions would be slightly different depending on the PIM. 
#1
Jim Nickerson
User 452
  • Total Posts : 6486
  • Reward points : 0
  • Joined: 2003/11/07 12:35:10
  • Location: San Diego, CA
  • Status: offline
Re: MCC configuration for the Explorer 16/32 2019/07/26 13:12:53 (permalink) ☄ Helpfulby dan1138 2019/07/26 21:58:06
5 (1)
There are two options for demo code on this page, choose the second "8/29/2016" for MCC examples
https://www.microchip.com/DevelopmentTools/ProductDetails/dm240001-2
#2
dan1138
Super Member
  • Total Posts : 3347
  • Reward points : 0
  • Joined: 2007/02/21 23:04:16
  • Location: 0
  • Status: offline
Re: MCC configuration for the Explorer 16/32 2019/07/26 13:26:49 (permalink)
0
mepartr
Anyone prepared an MCC configuration for the Explorer 16/32?  Working on a demo project and using the Explorer 16/32 development board.  Would really help to have an MCC configuration file available so I don't need to reverse-engineer the Explorer 16/32 to set pin functions and appropriately set configuration bits.  These functions would be slightly different depending on the PIM.

You don't mention which 16-bit or 32-bit controller you will use so it seems unlikely that anyone would create the MCC configuration file just for you.
 
The pin connections from the controller to the Explorer 16/32 PIM connector are not always one to one so Microchip has left it up to each developer to complete the documentation to verify which physical pin of the controller is actually connected to Explorer 16/32 resource. This is a tedious task and nobody where I work likes the way I do it.
 
The sample code from Microchip for the 16-bit controller PIMs for the Explorer 16/32 (DM240001-3) are hard from me to comprehend but maybe useful to you.
post edited by dan1138 - 2019/07/26 13:42:52
#3
Vegas Mike
New Member
  • Total Posts : 17
  • Reward points : 0
  • Joined: 2006/11/16 09:27:24
  • Location: Las Vegas, Nevada, USA
  • Status: offline
Re: MCC configuration for the Explorer 16/32 2019/07/26 14:22:01 (permalink)
0
Well, worth a shot.  When you say, "Just for me", I wonder how many others use the PIC24FJ1024GB610 PIM.  Microchip has all the Explorer 16/32 design files, so it would not be near as tedious for them to create the configuration as for us users.  The example code demos the LCD, LED, and slide potentiometer but does not use files in MCC format.
#4
dan1138
Super Member
  • Total Posts : 3347
  • Reward points : 0
  • Joined: 2007/02/21 23:04:16
  • Location: 0
  • Status: offline
Re: MCC configuration for the Explorer 16/32 2019/07/26 21:55:45 (permalink)
5 (1)
Pay attention to post #2 from Jim Nickerson!
#5
hkumar
Starting Member
  • Total Posts : 19
  • Reward points : 0
  • Joined: 2012/10/03 01:12:16
  • Location: 0
  • Status: offline
Re: MCC configuration for the Explorer 16/32 2019/08/11 23:39:34 (permalink)
0
I request you to use the Board Support Library http://ww1.microchip.com/downloads/en/DeviceDoc/boardSupportLibrary-1.0.0.mc3lib which will allow you to generate the code for the Explorer 16/32 boards and few other boards as well , Board Support Library will auto-configure the pins for you.
#6
Jim Nickerson
User 452
  • Total Posts : 6486
  • Reward points : 0
  • Joined: 2003/11/07 12:35:10
  • Location: San Diego, CA
  • Status: offline
Re: MCC configuration for the Explorer 16/32 2019/08/12 08:11:23 (permalink)
0
"you can lead a horse..." Smile: Smile
#7
Jump to:
© 2020 APG vNext Commercial Version 4.5