• AVR Freaks

Hot!mplab X in linux - can see but cannot program PIC32MZ / PIC32MX Starter kit in Hardware

Author
sl149q
New Member
  • Total Posts : 9
  • Reward points : 0
  • Joined: 2013/09/24 15:42:30
  • Location: 0
  • Status: offline
2019/07/26 09:55:01 (permalink)
0

mplab X in linux - can see but cannot program PIC32MZ / PIC32MX Starter kit in Hardware

I am trying to use MPLAB X in Linux Mint but cannot program either of my two Starter kit boards (PIC32MZ or PIC32MX Ethernet Starter kits).

When I plug them in, they show up in the Hardware tools under Microchip Kits. For example, I can see PIC32 ESK-II under the line Starter Kits (PKOB). But the small circle before that line stays Red, it does not turn Green. So I cannot select the device for programming. 

If I unplug that board, it is removed. Plugin the other and I get PIC32MZ EC Family, but again, still Red. 

What needs to be fixed in the system configuration to get this to work correctly?

Thanks!
#1

2 Replies Related Threads

    matta
    Senior Member
    • Total Posts : 137
    • Reward points : 0
    • Joined: 2006/11/15 14:05:02
    • Location: 0
    • Status: offline
    Re: mplab X in linux - can see but cannot program PIC32MZ / PIC32MX Starter kit in Hardwar 2019/08/07 14:53:07 (permalink)
    #2
    sl149q
    New Member
    • Total Posts : 9
    • Reward points : 0
    • Joined: 2013/09/24 15:42:30
    • Location: 0
    • Status: offline
    Re: mplab X in linux - can see but cannot program PIC32MZ / PIC32MX Starter kit in Hardwar 2019/08/07 19:32:47 (permalink)
    0
    matta
    Could it be related to this?
    https://www.microchip.com.../m1051283.aspx#1071746


    Yes, the hotplugscript was hanging.

    ATTR{idVendor}=="04d8", ATTR{idProduct}=="8107", MODE="666", GROUP="microchip", RUN+="%E{hotplugscript} add"

    Replaced with rules like this:
     
     
    ATTRS{idVendor}=="04d8", ATTRS{idProduct}=="00dd", MODE="666", GROUP="microchip",

    That works reasonably well.



    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5