• AVR Freaks

AnsweredPIC16F505 does not wake-up on pin change

Page: < 12 Showing page 2 of 2
Author
Blubb
New Member
  • Total Posts : 6
  • Reward points : 0
  • Joined: 2019/07/19 06:47:26
  • Location: 0
  • Status: offline
Re: PIC16F505 does not wake-up on pin change 2019/08/12 01:08:44 (permalink)
+1 (1)
So hello again :)

As simple as it is: It turned out the problem really was the stack. Rewriting the code to limit the number of calls solved the problem and the chip now works as expected!

Thank you all very much for your help and suggestions that I could use to continue forwards. 
#21
Page: < 12 Showing page 2 of 2
Jump to:
© 2020 APG vNext Commercial Version 4.5