• AVR Freaks

AnsweredHot!MCC I2C Library driver, why will it removed soon?

Author
vleroylr
Starting Member
  • Total Posts : 17
  • Reward points : 0
  • Joined: 2018/08/09 20:12:20
  • Location: 0
  • Status: offline
2019/07/22 08:54:01 (permalink)
0

MCC I2C Library driver, why will it removed soon?

I was working in MPLAB X IDE V5.15 and once I generated the MCC files for using I2C with the PIC18F45K40 I noticed in the file "i2c1.h" that there is a warning that states:
 
#warning "This version of the I2C driver will be removed soon and the correct driver to use is the Foundation Services Library driver"

 
So obviously I went back and tried the Foundation Services Library Driver, and found out that it is quite different, more basic, you can't watch the registers values as you could with the PIC10/PIC12/PIC17/PIC18 MCUs Library, there is less information about the generated functions... So my question is: Why this big change?, is there any other driver that will be removed aswell as the I2C driver?, should we all move and use the library foundation services libraries instead of the PIC10/PIC12/PIC17/PIC18 MCUs Library?
 
Thanks, I wait for everybody's comments. Víctor.
#1
katela
Super Member
  • Total Posts : 1814
  • Reward points : 0
  • Joined: 2013/06/11 05:25:18
  • Location: South Africa
  • Status: offline
Re: MCC I2C Library driver, why will it removed soon? 2019/07/22 09:17:22 (permalink)
0
That very strange from Microchip considering little information and options to setup the registers with the foundation driver.

Free online Microcontroller Tutorials and Projects for Hobbyists and students. From beginners to advanced. Website: www.studentcompanion.co.za
YouTube Tutorials: https://www.youtube.com/StudentCompanionSA
#2
vleroylr
Starting Member
  • Total Posts : 17
  • Reward points : 0
  • Joined: 2018/08/09 20:12:20
  • Location: 0
  • Status: offline
Re: MCC I2C Library driver, why will it removed soon? 2019/07/22 09:25:54 (permalink)
0
katela
That very strange from Microchip considering little information and options to setup the registers with the foundation driver.


Yes, I am interested on knowing why, I always follow microchip as in my job I always tell my costumers to use PIC MCUs, so it would be very handy to me to know what's the actual state. Thanks for your comment.
#3
PA91
Junior Member
  • Total Posts : 71
  • Reward points : 0
  • Joined: 2012/09/03 21:45:40
  • Location: 0
  • Status: offline
Re: MCC I2C Library driver, why will it removed soon? 2019/11/11 01:36:47 (permalink)
0
Hi,
MCC device library not just generates initialize function but also add other functions and even Foundation service generates I2C driver which was creating confusion in many people. So to make it come across these updates were made.
and it's available with the latest library release ( need not to switch to Foundation service )
PIC10 / PIC12 / PIC16 / PIC18 MCUs1.78.0 
 
 
#4
Mysil
Super Member
  • Total Posts : 3671
  • Reward points : 0
  • Joined: 2012/07/01 04:19:50
  • Location: Norway
  • Status: offline
Re: MCC I2C Library driver, why will it removed soon? 2019/11/11 08:35:24 (permalink) ☼ Best Answerby vleroylr 2019/11/28 09:07:49
+3 (3)
Hi, Victor and others.

It have happened, in version 1.78 of device library for PIC10-PIC12-PIC16-PIC18,
the task queue driver for I2C have disappeared.

Instead, there is a variant of the previous Foundation Services driver.
There are significant improvements, and a differences in location and naming of some files,
and a number of changes in symbols and function names, mostly some more uppercase letters.

The driver design is just as obscure and undocumented as before.
Also the code in  i2c_master.c and i2c_master.h,
isn't a complete driver, it is a transfer engine and some building blocks for:
"Write your own driver."

There is a table with a number of callback function pointers,
so when something interesting happen, the transfer engine will call one of those pointers,
where you are supposed to put in a function to take care of whatever may be needed.
There are some functions provided, so when everything go well, it may work as expected.

In the current release of the library, hardware interface to MSSP registers,
is generated in the same source file,
so it might be possible for inline optimizations to work with optimization level 1
in free mode in version 2.xx of  XC8 compiler.

In addition to the transfer engine,
there is also a subdirectory with  i2c_master_example.c  and  i2c_master_example.h.
They contain application interface functions similar to what is provided by
i2c_simple_master.c  and  i2c_simple_master.h

While the transfer engine in i2c_master.c  may be configured to work in non-blocking mode using interrupts,
all the application interface functions in i2c_master_example.c and i2c_simple_master.c  degenerate to blocking mode, waiting for every transfer to complete before returning.

This may be o.k. for many simple programs using I2C sensors,
and in many PIC16 devices with only one interrupt priority level and small hardware stack, interrupt I2C driver may be more nuisance than benefit.

There was some other bad behaviour in previous versions of Foundation Services driver that have been removed.
In case of a slave not responding due to beeing busy or disconnected,
previous versions of foundation services driver did retry the address write without limitation or timeout, causing the bus to be jammed for any other devices using the same lines, and making the program hang without returning to caller.
This also make it impossible to scan a bus for available devices.

See this thread and the link to microforum
https://www.microchip.com/forums/FindPost/1117381


The task queue driver for I2C in previous versions of device libraries,
also have mistakes and limitations.
A design mistake in application interface to task queue use local structure in API routines as part of task queue entries, such that if more than one read and one write transfer is requested, they may destroy each other.
Also task queue entries was released immediately when a transfer was started,
making difficulties for retries or recovery.

A rewrite of the task queue I2C driver is here:
https://www.microchip.com/forums/FindPost/978822
There are versions of the driver that may run on many different families of PIC devices,
PIC16 and PIC18 with MSSP peripheral,
some PIC24 and dsPIC33 devices,
and PIC32MX  devices.
Driver is also running on PIC32MZ.
Generally, it is not difficult to port the driver code to different devices in the same families, even if it cannot be generated by MCC.
They all provide the same application interfaces for all devices.
There is also a blocking bitbanging I2C driver for PIC32MM devices that have no functional I2C peripheral, it also have the same application interface.

I might publish a blocking, non-interrupt driver for use with PIC16 devices with MSSP peripheral. It will provide the same application interface as for other examples in the same thread.
Application example code in  projects in the thread is big and messy,
intended to exercise a lot of different usage.  

Regards,
    Mysil
#5
Jump to:
© 2020 APG vNext Commercial Version 4.5