• AVR Freaks

Hot!Identifying Pin-1 on PIC32MX470F512L Controller

Author
_pA89
New Member
  • Total Posts : 29
  • Reward points : 0
  • Joined: 2017/06/06 12:39:37
  • Location: India
  • Status: offline
2019/07/20 02:36:59 (permalink)
0

Identifying Pin-1 on PIC32MX470F512L Controller

There are two holes - how to identify pin-1 on the controller
---> Should we take bigger hole || smaller hole as Reference...
In below image is the Required Controller

Attached Image(s)

#1

9 Replies Related Threads

    TS9
    Super Member
    • Total Posts : 793
    • Reward points : 0
    • Joined: 2010/05/07 10:52:22
    • Status: offline
    Re: Identifying Pin-1 on PIC32MX470F512L Controller 2019/07/20 03:33:21 (permalink)
    0
    It should be from small hole.

    Also Watch closely , there is small cut at the edge of the chip

    I don't this PIC but it should be same (small hole).
    post edited by TS9 - 2019/07/20 03:40:39
    #2
    crosland
    Super Member
    • Total Posts : 1673
    • Reward points : 0
    • Joined: 2005/05/10 10:55:05
    • Location: Warks, UK
    • Status: offline
    Re: Identifying Pin-1 on PIC32MX470F512L Controller 2019/07/20 04:10:45 (permalink)
    0
    RTFM - try reading the data sheet.
    #3
    _pA89
    New Member
    • Total Posts : 29
    • Reward points : 0
    • Joined: 2017/06/06 12:39:37
    • Location: India
    • Status: offline
    Re: Identifying Pin-1 on PIC32MX470F512L Controller 2019/07/20 04:14:19 (permalink)
    0
    Thanks for the Fast Reply, Yes I Can Confirm the Small Cut
     P.S. : RTFM- Shows only single Hole... 
    post edited by _pA89 - 2019/07/20 04:21:59
    #4
    _pA89
    New Member
    • Total Posts : 29
    • Reward points : 0
    • Joined: 2017/06/06 12:39:37
    • Location: India
    • Status: offline
    Re: Identifying Pin-1 on PIC32MX470F512L Controller 2019/07/26 12:27:28 (permalink)
    0
    270719: Confirmed - Smaller Hole is the Reference(Able to Program Device Using PICKit-3) -Thanks for the Answer/Clearing Doubt @ TS9 Smile: Smile
     
    P.S. : RTFM- Shows only single Hole(BUG?)... In Low Resolution-Non-Professional Image - cuts seem to appear on Every Edge -- With (Microchip Logo Orientation && Hole) we can establish Pin-1 at smaller Hole. But Still It will be Confusing/Frustrating...
     
    #5
    NKurzman
    A Guy on the Net
    • Total Posts : 17943
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: online
    Re: Identifying Pin-1 on PIC32MX470F512L Controller 2019/07/26 13:48:50 (permalink)
    0
    The lower left corner has the notch in your picture.
    #6
    ric
    Super Member
    • Total Posts : 24285
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: Identifying Pin-1 on PIC32MX470F512L Controller 2019/07/26 14:54:02 (permalink)
    0
    I think they are referring to the corners in the drawing in the datasheet.
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #7
    NKurzman
    A Guy on the Net
    • Total Posts : 17943
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: online
    Re: Identifying Pin-1 on PIC32MX470F512L Controller 2019/07/26 15:29:45 (permalink)
    0
    page 339 and page 4.
    #8
    _pA89
    New Member
    • Total Posts : 29
    • Reward points : 0
    • Joined: 2017/06/06 12:39:37
    • Location: India
    • Status: offline
    Re: Identifying Pin-1 on PIC32MX470F512L Controller 2019/08/18 23:40:45 (permalink)
    0
    Device Identification: PIC32MX470F512L-I/PF  (14x14x1)mm TQFP
     
     
    1. It cant be inferred from Pg-7     as it shows only 1-hole, cuts appear to be on all sides
    2. It cant be inferred from Pg-337 as it shows only 1-hole, cuts appear to be on all sides
        2.1. NOTE-2: Chamfers at corners are optional, size may vary
     
    P.S. : Is there a Valid Solution to current Question -Considering Datasheet ?

    Attached Image(s)

    #9
    Gort2015
    Klaatu Barada Nikto
    • Total Posts : 3315
    • Reward points : 0
    • Joined: 2015/04/30 10:49:57
    • Location: 0
    • Status: offline
    Re: Identifying Pin-1 on PIC32MX470F512L Controller 2019/08/19 02:10:47 (permalink)
    0
    Any color chip as long as it is black.

    MPLab X playing up, bug in your code? Nevermind, Star Trek:Discovery will be with us soon.
    https://www.youtube.com/watch?v=Iu1qa8N2ID0
    + ST:Continues, "What Ships are Made for", Q's back.
    #10
    Jump to:
    © 2019 APG vNext Commercial Version 4.5