• AVR Freaks

ICD3 short circuit

Author
mirch25
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2019/07/17 04:53:20
  • Location: 0
  • Status: offline
2019/07/20 02:14:43 (permalink)
0

ICD3 short circuit

Hello Microchip community!
 
This is my first post on this forum so please be gentle to me :)
 
Last week I get in my hand ICD3 which was not recognized by windows computer, not even shown in device manager. Later I have recognized that it is on one side pretty hot. I have open the ICD3 box, and found an IC which is very hot - it is "2014 86M A3JN" (picture in attachment).
 
I have try to look for some spare ICs and datasheet, but what I have found were only calculators :) Can someone please provide me the source of the datasheet or something, that I see if is reperable.
 
Thanks!
 
 

Attached Image(s)

#1

3 Replies Related Threads

    du00000001
    Just Some Member
    • Total Posts : 3840
    • Reward points : 0
    • Joined: 2016/05/03 13:52:42
    • Location: Germany
    • Status: offline
    Re: ICD3 short circuit 2019/07/22 09:50:07 (permalink)
    +1 (1)
    "2014" is expected to be
    TI TPS2014 (.66A POWER DIST SWITCH 8-SOIC)
     
    Dug up some fancy document as well - too large to upload here - with some luck, the following link will work:
    https://www.dropbox.com/l/scl/AADneBL0cJcBlKq4m4-5A5tKOdcYwMVDRKs

    PEBKAC / EBKAC / POBCAK / PICNIC (eventually see en.wikipedia.org)
    #2
    NKurzman
    A Guy on the Net
    • Total Posts : 18850
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: ICD3 short circuit 2019/07/22 14:43:35 (permalink)
    0
    How Old is the IC3?  Microchip may fix it.
     
    https://www.microchip.com/cisar/Home.aspx
    #3
    mirch25
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2019/07/17 04:53:20
    • Location: 0
    • Status: offline
    Re: ICD3 short circuit 2019/07/22 23:03:19 (permalink)
    0
    I dont know how old it is ... Assy# number is 10-00421-RC if this helps anything.
     
    Thanks "du00000001" for provided link for datasheet! grin: grin
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5