• AVR Freaks

Hot!PIC16F18326 cannot disable MSSP1 ints using MCC

Author
teranz
Starting Member
  • Total Posts : 82
  • Reward points : 0
  • Joined: 2019/03/06 21:45:25
  • Location: 0
  • Status: offline
2019/07/18 08:39:05 (permalink)
0

PIC16F18326 cannot disable MSSP1 ints using MCC

Hi:
I am using both the MSSP channels of a PIC16F18326 mpu.  Both channels appear to work fine, but using MCC Version: 3.85.1     in MPLAB X IDE v5.20 does not allow me to disable the MSSP1 interrupts visually.  Any clues as to what is wrong or I am missing?  I have seen similar happen using MPLAB X IDE v5.15 and an earlier MCC version.
 
Thanks

Attached Image(s)

#1

4 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 18779
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: online
    Re: PIC16F18326 cannot disable MSSP1 ints using MCC 2019/07/18 09:21:03 (permalink)
    0
    Since the is an MCC is you should have posted (or Cross Posted) it there.
    #2
    teranz
    Starting Member
    • Total Posts : 82
    • Reward points : 0
    • Joined: 2019/03/06 21:45:25
    • Location: 0
    • Status: offline
    Re: PIC16F18326 cannot disable MSSP1 ints using MCC 2019/07/18 10:32:19 (permalink)
    0
    OK... I see that, I`m not great with forums.  I would try it by I`m not sure how and I don`t want to cause more  issues.
    #3
    PA91
    Junior Member
    • Total Posts : 71
    • Reward points : 0
    • Joined: 2012/09/03 21:45:40
    • Location: 0
    • Status: offline
    Re: PIC16F18326 cannot disable MSSP1 ints using MCC 2019/11/11 01:01:46 (permalink)
    0
    Hi teranz,
     
    I am not able to understand your question and what's the solution that you are looking for.
     
    From the MCC side,
    1) SPI in Master mode doesn't support interrupt ( even though you can check the Interrupt). "Notifications" tab shows the message on the same.
    2) SPI in Slave mode support Interrupt.
     
    In any case, i am able to "check or uncheck" the MSSP1 interrupts.
     
    while adding the query please add the library versions that are been used. That help to verify.
     
     
     
     
    #4
    teranz
    Starting Member
    • Total Posts : 82
    • Reward points : 0
    • Joined: 2019/03/06 21:45:25
    • Location: 0
    • Status: offline
    Re: PIC16F18326 cannot disable MSSP1 ints using MCC 2019/11/11 07:03:20 (permalink)
    0
    Hi:
    I have worked around this issue so it is not a show-stopper, but the fact is the MCC does not allow me to change the interrupt boxes.
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5