• AVR Freaks

[DELETE PLEASE][USB][PIC32MM0256GPM064] USB CDC example

Author
LuisNascimento
New Member
  • Total Posts : 6
  • Reward points : 0
  • Joined: 2018/06/28 07:05:07
  • Location: 0
  • Status: offline
2019/07/17 04:04:13 (permalink)
0

[DELETE PLEASE][USB][PIC32MM0256GPM064] USB CDC example

Hello, 
I have made a direct connection from the USB pins to the PIC32MM0256GPM064 and  the MCC generated the CDC example, open a terminal to try to get a response but it doesn't work. Is there something I'm missing?! 
Attachments are not available: Download requirements not met  
Regards,
post edited by LuisNascimento - 2019/07/17 07:56:11

Attachment(s)

Attachments are not available: Download requirements not met
#1

3 Replies Related Threads

    oliverb
    Super Member
    • Total Posts : 204
    • Reward points : 0
    • Joined: 2009/02/16 13:12:38
    • Location: 0
    • Status: offline
    Re: [USB][PIC32MM0256GPM064] USB CDC example 2019/07/17 04:53:57 (permalink)
    0
    Are you supplying VUSB3V3 with 3.3V?
    Is your clock configured correctly?
    #2
    LuisNascimento
    New Member
    • Total Posts : 6
    • Reward points : 0
    • Joined: 2018/06/28 07:05:07
    • Location: 0
    • Status: offline
    Re: [USB][PIC32MM0256GPM064] USB CDC example 2019/07/17 05:00:27 (permalink)
    0
    oliverb
    Are you supplying VUSB3V3 with 3.3V?
    Is your clock configured correctly?




     
    Yes and yes
    Attachments are not available: Download requirements not met

    Attachment(s)

    Attachments are not available: Download requirements not met
    #3
    LuisNascimento
    New Member
    • Total Posts : 6
    • Reward points : 0
    • Joined: 2018/06/28 07:05:07
    • Location: 0
    • Status: offline
    Re: [USB][PIC32MM0256GPM064] USB CDC example 2019/07/17 07:55:22 (permalink)
    0
    Problem solved! The USB connector was making a bad connection, I replace that and everything worked Smile: Smile , so much time on this and was a bad connection....mad: mad
     
    This thread can be closed, thanks for the response oliverb btw :) 
    #4
    Jump to:
    © 2019 APG vNext Commercial Version 4.5