• AVR Freaks

Helpful ReplyHot!Problem finding data about ODCx register

Author
vra
Starting Member
  • Total Posts : 72
  • Reward points : 0
  • Joined: 2014/07/14 18:35:19
  • Location: 0
  • Status: offline
2019/07/16 17:47:02 (permalink)
0

Problem finding data about ODCx register

Hi all, how are you?. I'm trying to find data on the datasheet and the respective Reference manual of the PIC24EP512XXX and it seems impossible to find which ports has that functionality. If I see inside the .h header of the respective PIC24EP512GU810 and there isn't nothing defined for ODCB register which is the port what I wanna use so the apparently obvious conclusion is that port doesn't have the functionality for open drain pin but...it is possible to find that information in some paper?.
#1
NKurzman
A Guy on the Net
  • Total Posts : 17623
  • Reward points : 0
  • Joined: 2008/01/16 19:33:48
  • Location: 0
  • Status: offline
Re: Problem finding data about ODCx register 2019/07/16 19:01:35 (permalink) ☄ Helpfulby vra 2019/07/16 20:12:54
4.5 (2)
The Reference Manual doe not tell you what features a specific chip has.
 
http://ww1.microchip.com/downloads/en/DeviceDoc/70616g.pdf
 
Page 115
TABLE 4-56: PORTB REGISTER MAP
That Port does not appear to have that feature.
 
 
 
 
#2
vra
Starting Member
  • Total Posts : 72
  • Reward points : 0
  • Joined: 2014/07/14 18:35:19
  • Location: 0
  • Status: offline
Re: Problem finding data about ODCx register 2019/07/16 20:12:41 (permalink) ☄ Helpfulby Jim Nickerson 2019/07/17 07:24:30
5 (1)
NKurzman
The Reference Manual doe not tell you what features a specific chip has.
 
http://ww1.microchip.com/downloads/en/DeviceDoc/70616g.pdf
 
Page 115
TABLE 4-56: PORTB REGISTER MAP
That Port does not appear to have that feature.



Yeah...I think I need to read a little bit more
#3
Jim Nickerson
User 452
  • Total Posts : 6128
  • Reward points : 0
  • Joined: 2003/11/07 12:35:10
  • Location: San Diego, CA
  • Status: offline
Re: Problem finding data about ODCx register 2019/07/17 07:25:48 (permalink)
4 (1)
Valery
NKurzman
The Reference Manual doe not tell you what features a specific chip has.
 
http://ww1.microchip.com/downloads/en/DeviceDoc/70616g.pdf
 
Page 115
TABLE 4-56: PORTB REGISTER MAP
That Port does not appear to have that feature.



Yeah...I think I need to read a little bit more


Well said !
#4
Jump to:
© 2019 APG vNext Commercial Version 4.5