• AVR Freaks

Hot!Can I use MPLAB-X to view the internal SDRAM 32MB memory (for the PIC32MZ1025DAG169)

Author
cbeif
Starting Member
  • Total Posts : 58
  • Reward points : 0
  • Joined: 2012/05/09 14:28:30
  • Location: 0
  • Status: offline
2019/07/10 11:43:47 (permalink)
0

Can I use MPLAB-X to view the internal SDRAM 32MB memory (for the PIC32MZ1025DAG169)

I am having alot of trouble writing and reading to the SDRAM.
Is there a way to use the debugger to see what's inside the internal DDR2 SDRAM?
 
I don't see any of the "Target Memory Views" which contain the address of 0x88000000.
#1

4 Replies Related Threads

    crennolet
    Super Member
    • Total Posts : 144
    • Reward points : 0
    • Joined: 2012/03/15 09:51:58
    • Location: 0
    • Status: offline
    Re: Can I use MPLAB-X to view the internal SDRAM 32MB memory (for the PIC32MZ1025DAG169) 2019/07/11 10:15:40 (permalink)
    0
    OK, I'll bite.
    Are you sure you have the part right? The specs sheet for the part you say you have says "256K" for internal static ram.
    #2
    jdeguire
    Super Member
    • Total Posts : 487
    • Reward points : 0
    • Joined: 2012/01/13 07:48:44
    • Location: United States
    • Status: offline
    Re: Can I use MPLAB-X to view the internal SDRAM 32MB memory (for the PIC32MZ1025DAG169) 2019/07/11 10:29:35 (permalink)
    +1 (1)
    Hmmm...the webpage for your part (https://www.microchip.com/wwwproducts/en/PIC32MZ1025DAG169) is recommending using the PIC32MZ1025DAR169 instead and no longer indicates that your part has internal DDR2 memory (though the datasheet says it does).  Perhaps the early parts are flaky or defective in some way.
    #3
    cbeif
    Starting Member
    • Total Posts : 58
    • Reward points : 0
    • Joined: 2012/05/09 14:28:30
    • Location: 0
    • Status: offline
    Re: Can I use MPLAB-X to view the internal SDRAM 32MB memory (for the PIC32MZ1025DAG169) 2019/07/11 11:21:07 (permalink)
    0
    Ahh rats, I have been struggling for about 3 weeks to get the internal SDRAM to work,
    I guess I now know why. (I wish there was a reason given for the obsolescence)
    #4
    scottoc
    New Member
    • Total Posts : 6
    • Reward points : 0
    • Joined: 2012/08/23 09:03:13
    • Location: 0
    • Status: offline
    Re: Can I use MPLAB-X to view the internal SDRAM 32MB memory (for the PIC32MZ1025DAG169) 2019/08/21 15:13:29 (permalink)
    +1 (1)
    The PIC32MZ1025DAG169 internal 32MB DDR2 SDRAM works fine. There are many graphics demo projects in Harmony that use this part with the SDRAM. The newer PIC32MZ1025DAR169 just fixes many of the errata on the DAG family of parts. Some compatibility issues forced them to release the new parts with new part numbers. So for a new project it is recommended to use the new part. But the old part does work. You can compare the 2 errata docs on their web site to see what was fixed.
     
    What version of MPLAB X IDE are you using? I know that at least version 4.20 and later have a Target Memory View Window for External DDR Memory. It shows data beginning at DDR2 SDRAM Physical address of 0x80000000. However, it is not clear to me if or how this data gets updated when the debugger halts. I suspect that 32MB is way too much to load every time the debugger halts. You may have to click the "Read Device Memory" button in the window to refresh it when you need to see it.
     
    Note: although the PIC32MZ1025DAG169 datasheet shows it has "internal" 32MB DDR2 SDRAM, it is actually a stacked die so is technically external to the PIC32MZ die. Just wanted to clarify due to the conflicting usage above of words internal vs. external.
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5