• AVR Freaks

Hot!BM62 MFB button configuration ui settings

Author
Ali_king
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2018/10/30 07:09:00
  • Location: 0
  • Status: offline
2019/07/10 07:17:47 (permalink)
0

BM62 MFB button configuration ui settings

Hello,
 
I am looking for a way to arrange the UI settings for the MFB pin. i want it enabled as a button. for a short press it should  wake up the bm62 from being off and then a long press should start bluetooth pairing (a2dp). I tried and failed several time to set this up using the ui tool. If anyone has a similar setup or knows how to push me in the right direction any help would be greatly appreciated. 
 
Thanks,
Alister 
 
Note to any looking at using the bm62:
I find the BM62 UI tool very clunky and it is a pain to use. There is unclear English and the system is very confusing. Simple changes like configuring buttons require an entire regeneration of all the files.  
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5