PWM 1, 3 and 4 pins not working on dsPIC33EP
Hello everyone, Im developing a project on dsPIC33EP512GM710 and everything ok but im surprised when I was configuring the PWM module, the pins associated does not work, only on PWM2 I got signal, JTAG Off is set and tried everything, disabling PMP module, ANSEL, TRIS, PWM unlock etc, the pins not work in I/O mode so the problem is the pins configuration but I tried al I know, the pins are RB10, RB11, RB14 , RB15 and possibly any others , on datasheet that pins are marked as Output so I dont undestand, can anyone help me? Thank you very much