• AVR Freaks

Hot!Customer Linker setup PIC24FJ

Page: < 12 Showing page 2 of 2
Author
jtzeng
Super Member
  • Total Posts : 467
  • Reward points : 0
  • Joined: 2003/11/07 12:42:20
  • Status: offline
Re: Customer Linker setup PIC24FJ 2019/07/10 08:53:12 (permalink)
+1 (1)
This is what I needed.  I can see how to do it in the linker script, but I like this much better.
Thanks.

John Zigrang
JTZ Engineering, Inc.
#21
ToddA
New Member
  • Total Posts : 19
  • Reward points : 0
  • Joined: 2018/05/15 14:04:18
  • Location: 0
  • Status: offline
Re: Customer Linker setup PIC24FJ 2019/07/12 05:57:19 (permalink)
0
Sounds like you need a bootloader - take a look at AN1157. Not sure if the code is customizable, but it could be a starting point.
#22
Page: < 12 Showing page 2 of 2
Jump to:
© 2019 APG vNext Commercial Version 4.5