• AVR Freaks

Hot!LoRa Development Utility for the LoRa evalution kit 900 - mysql

Author
stephen_odonnell
New Member
  • Total Posts : 1
  • Reward points : 0
  • Status: offline
2019/07/08 11:31:57 (permalink)
0

LoRa Development Utility for the LoRa evalution kit 900 - mysql

Hi, 
I am new to the LoRa evalution Kit 900 and I was wondering if someone knew if it is possible to access the MySql Database used by the application with an other software such as "phpMyAdmin" or "MySql". I have tried accessing it via these two software but so far it hasn't worked. Does anyone have an idea to make it work? 
 
stephen O.
 Thank you in advance for your answer(s).
 
PS: I currently working on a LoRa project as part of an intership.
#1

1 Reply Related Threads

    mustafaakgul
    New Member
    • Total Posts : 7
    • Reward points : 0
    • Joined: 2020/01/29 03:16:08
    • Location: 0
    • Status: offline
    Re: LoRa Development Utility for the LoRa evalution kit 900 - mysql 2020/01/30 05:14:30 (permalink)
    0
    Did you try to use linux machine or docker?
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5