• AVR Freaks

Hot!Cannot reprogram PIC10F200

Page: < 12 Showing page 2 of 2
Author
mbrowning
Just a Member
  • Total Posts : 1457
  • Reward points : 0
  • Joined: 2005/03/16 14:32:56
  • Location: Melbourne, FL
  • Status: offline
Re: Cannot reprogram PIC10F200 2019/07/12 07:32:28 (permalink)
+1 (1)
acharnley
Wouldn't the chip have used a full erase the first time it's programmed?

The chips ship erased. A failed full erase at that point would look the same as a successful full erase.

Oh well - there's always next year
#21
ric
Super Member
  • Total Posts : 23200
  • Reward points : 0
  • Joined: 2003/11/07 12:41:26
  • Location: Australia, Melbourne
  • Status: offline
Re: Cannot reprogram PIC10F200 2019/07/12 14:36:01 (permalink)
+1 (1)
acharnley
Wouldn't the chip have used a full erase the first time it's programmed?

If it's already blank, it wouldn't matter that it didn't work.

I also post at: PicForum
Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
NEW USERS: Posting images, links and code - workaround for restrictions.
To get a useful answer, always state which PIC you are using!
#22
Page: < 12 Showing page 2 of 2
Jump to:
© 2019 APG vNext Commercial Version 4.5